Part Number: BQ24401 Tool/software: Hello,
I'm looking for guidance on selecting a Texas Instruments IC for a Ni-MH battery pack with a nominal 12V/3Ah rating, composed of 10 cells of 1.2V each (Ni-MH SC 3000mAh). Here are the primary requirements for…
Part Number: BQ24401 Other Parts Discussed in Thread: BQ25798 , Tool/software: Hello E2E Experts,
Good day.
I was wondering if this would be a suitable charger for solar applications.
If so I noticed on the data sheet that the schematic of the sample design…
Other Parts Discussed in Thread: BQ24401 , BQ25172 Hi team,
our customer is asking if we have alternative solution for CN3085.
I have promoted our BQ24401 device but wonder if we have any newer solution.
Please comment if you have any suggestion, thanks…
Part Number: BQ24401 Other Parts Discussed in Thread: BQ25172 , BQ25171-Q1 Hi support team,
Our customer want to know the quiescent current of BQ24401 in case the device is disabled.
There is no that kind of data in the datasheet.
Could you let me know…
Part Number: BQ24401 Howdy,
I'm working on a design to use the BQ24401 to charge a 3-cell NiMH battery. I think I may be confused on the operation and was looking for some clarification to ensure that I understand how things should work. It seems like…
Part Number: BQ24401 Other Parts Discussed in Thread: BQ25171-Q1 , Hello,
We are starting on a new design for our cellular tracking device. It will use a rechargeable NiMH battery (about 500mAH) .
Can you suggest an option for battery charger IC that can…
Part Number: BQ24401 Other Parts Discussed in Thread: BQ2000 The customer is looking for a charging IC for NiMH.
Battery specifications are
- Voltage: 4.8V (NiMH 4-Cell) - Capacity: 1450mAh
Interface: Standalone
What is the recommended charging IC? If it…
Part Number: BQ2000 Other Parts Discussed in Thread: BQ24401 Hello, how do you do?
May I have some questions below regarding to the BQ2000 or BQ24401 charging ICs ?
Q1) Can both ICs be used for 2 cells NiMH battery charging ? If so, changing the voltage…
Part Number: BQ24401 I'm using the BQ24401 to charge 3s NiMH batteries 3.6V 1600mAH.
I'm using a 5V input to the charging circuit this voltage drops to 4.5 though the diode.
Circuit is set up for a max current of 500mA.
Everything seems to be…
Part Number: BQ24401 Hi,
We've had a 6S NiMH charge circuit designed externally using the BQ24401. As far as I can tell, the circuit matches that in Figure 7. of http://www.ti.com/lit/ds/symlink/bq24401.pdf with the VBAT resistor divider changed to…