Part Number: BQ24401 Other Parts Discussed in Thread: BQ2000 The customer is looking for a charging IC for NiMH.
Battery specifications are
- Voltage: 4.8V (NiMH 4-Cell) - Capacity: 1450mAh
Interface: Standalone
What is the recommended charging…
Part Number: BQ24401 Hi,
I’m not sure why these value is different though both devices are for NiMH 4cell max in product list in TI.com. Or is this typo in either one of the two?
Best Regards,
Satoshi / Japan Disty
Part Number: BQ24401
Hi,
I am planning to use BQ24401 NiMH battery charger IC for charging single cell NiMH battery (nominal voltage is 1.2V). In the datasheet it is showing BQ24401 can charge 3 cell NiMH cell (page 10). Can BQ24401 be used to charge…
Part Number: BQ24401 Other Parts Discussed in Thread: TPS3839 Hi, Customer is considering bq24401. ・Battery type is Ni-MH. ・1cell / 2cell ・0.2C charge ・Vin=5V
However, bq24401 has no dry cell protection. Could you tell me dry cell protection solution…
Part Number: BQ24401 Other Parts Discussed in Thread: BQ2000T ,
Hi Team, Is there any difference between bq24401 and bq2000T for NiMH charger? It seems similar device as NiMH charger and I would like to know the difference if there is. Best Regards…
Part Number: BQ24401 Hi,
I understand that the BAT pin is connected to battery so the battery voltage is applied to BAT pin at no AC adapter connected, but I believe that there is no problem. However the Abs max of BAT pin is VCC and this is incorrect…
Part Number: BQ2000 Other Parts Discussed in Thread: BQ24401 Hello, how do you do?
May I have some questions below regarding to the BQ2000 or BQ24401 charging ICs ?
Q1) Can both ICs be used for 2 cells NiMH battery charging ? If so, changing the voltage…
Part Number: BQ24401 Dear Team,
We are looking for NiMH battery charger with Q grade.
The use case is 5Vin to 4.8V_battery@0.3C charging current. Battery pack spec: NiMH Battery / 4.8V /600mAh
Please contact with me offline if we have this solution…