Part Number: BQ24600 Hello to TI support team ,
I have question according status state in the following real battery charger scenario :
1. Proper Charging 3S battery , 2A charging up to 11.5V battery voltage dis balance protection operated --…
Part Number: BQ24600 Other Parts Discussed in Thread: BQ24610 Hello to Ti support team ,
I have question according back up timer integrated in bq24600 ,
1. According to SLUS891B page 8 internal 5h safety timer is in range 4.25h<T<5.75h , How set…
Part Number: BQ24600 Hello to TI team ,
1. I would like to know leakage current to the IC from Battery after charge procedure completed (IC supply present) ?
2. I would like to know leakage current to the IC from Battery without P.S connection …
Part Number: BQ24600 Hi,
The datasheet of the BQ24600 (SLUS891B –FEBRUARY 2010–REVISED NOVEMBER 2014)
states in Chapter 5 (page 3) in the Pin function table that the STAT Pin No. 3 is an Input. But that should be Output, right ?
BR
Normen
Part Number: BQ24600 SCH as below, 4 Li cells,VDD_ADPT is 24V, the charging current can not be changed when I change the V-iset or the R-sense, when I set the max current of the power supply unit at 3A, the charge current is 3A, and when I set the max…
Part Number: BQ24600 I am trying to charge a 4S1P, 18650 cell battery pack with BMS @ aprox 1amp current OUTPUT WAVEFORMS FOR THE BATTERY CHARGING CIRCUIT..pptx . wave forms and schematic are as per the presentation attached.
the output voltage keeps…
Part Number: BQ24600
Hi team,
I have a customer who saw the "Q4,Q5" for BQ24600's design as picture shows(btw, the screenshot was excerpted in BQ24600's datasheet), but he cannot find the part number SiR426D N in Vishay's official website or product…
Hi Kedar,
I actually have the STAT pins of three bq24600s on my board tied together, so I only see the LED blinking when all three chargers have completed charging, with one or more of them having experienced an apparent timer fault. If only one charger…