Part Number: BQ24610 Hi Teams,
The customer is using BQ24610 for robot applications and they have a dual battery solution. Below is SCH. Can you please help confirm if there are any issues? Thank you.
Part Number: BQ24610 I have designed a schematic for the BQ24610 charger IC. Part of my requirements for this system include being able to charge to a full pack voltage (25.2V for my 6S system) as well as a nominal 21.6V level for storage.
I have implemented…
Part Number: BQ24610 Hi Teams
There are requirements for the VGS of these two MOS transistors of BQ24610. The input terminal is 24V, and the driving voltage of the G-pole is ACDRV. What are the maximum and minimum voltages output by this pin?
Part Number: BQ24610 Hi team,
The following customers are using the BQ24610. Please review the schematic to see if there are any issues. Thank you.
9Ah 12.6V battery, with a pre-charge/cut-off current of 130mA
Icharge-VISET1/(20*0.01)3.3*(33/…
Part Number: BQ24610
Hi , What scenarios and products is BQ24610 specifically applied to? Which product categories see the most extensive usage? Could you offer relevant application cases? I noticed a medical device application…
Part Number: BQ24610 Hello TI,
I have a problem on BQ24610 on the circuit board.
[Urgent]
We need to have a support for the batch production schedule.
[Problem statement]
The issue is that BQ24610 keeps pulling down the ACDRV even if the…
Part Number: BQ24610 My system consists of a BQ24610 configured to charge a 6S lithium-ion battery pack with a power path. The battery pack voltage is 25.2 V and the charging current is 500 mA. The main power supply (input voltage to the BQ24610) is 28…
Part Number: BQ24610 Other Parts Discussed in Thread: BQ77915 , Hello,
I would like to confirm whether my system can operate as intended with the described configuration.
I am using BQ24610 to charge a 4S6P Li-ion pack (~18Ah, max discharge 60A).…
Part Number: BQ24610 Hi everybody,
I'm currently developing a battery charger board using the BQ24610 charger IC. The board has to charge 4 lithium-ion batteries connected in series. The charging current is set to 2 amps with a trimmer.
During the…
Part Number: BQ24610 Hello,
I wish to verify there's no issue with the voltage feedback network in my application.
I'm using an external battery pack, and due to system requirements, the upper resistor next to BQ24610 will be 90K, and on the battery…