Part Number: BQ24610EVM Hi
I use BQ24610EVM found :supply 12V DC,change the Charge current from 3A to 8A,the Voltage leave(PIN3 ---GND) is different ,and the MOS Q1 and Q2 are very hot when BQ24610EVM works at the high Charge current condition,such as…
Part Number: BQ24610EVM Other Parts Discussed in Thread: BQ24610 Hi Team,
Could you kindly recommend how to choose D1 with the max 1.05A charging current for 3s?
Thanks and best regards,
Jamie
Part Number: BQ24610EVM Hi,
I notice there is a Cff with feedback resistor.
Is this Cff for filter purpose? If it is, it looks like a HPF.
Should this one be LPF (parallel with R1) or this is not for filter purpose.
Thanks
Part Number: BQ24610EVM Other Parts Discussed in Thread: BQ24610 Hello,
I have a question about TVS diodes for use in the standard BQ24610EVM circuit layout.
Would it be good to connect a TVS diode at the connector of the ACPWR pin? I made provision…
Hi, Christian
Thank for response.
Is there any answer to Question 1 and Question 2 above?
The customer said that they reflected the layout guide contents in the datasheet and EVM as much as possible, but do you think the layout is the main cause?
If so…
Part Number: BQ24610EVM-603 Hi Expert :
We need application which is 7s~15s charger IC.
After check TI website, I find out BQ24610EVM-603 solution, but this EVM already stop producing.
Is it possible to apply this EVM ?
…
Part Number: BQ24610EVM Other Parts Discussed in Thread: BQ24610 Hi,
I have replicated the BQ24610EVM circuit on a custom PCB. When I power the circuit on (CE LOW) everything looks ok, i.e. PG indicates power is good. As soon as I turn on CE (HIGH), PG…
Part Number: BQ24610EVM Hi,
Our customer wants the shematic and pcb files of BQ24610-EVM. Would ypu please help provide the shematic and pcb files designed by Altium Designer software? So they can speed up the design. thanks.
Part Number: BQ24610 Other Parts Discussed in Thread: , TPS65987D Hi Team,
I will be happy to get your help with the bring up of BQ24610EVM.
I have connected 5 Bat (Sumsung INR18650-25R - data sheet attached) to the BQ24610EVM:
It seems that the BQ24610…
Hi Chris,
We haven’t heard back from you. We are assuming you were able to resolve your issue. If not, just post a reply below or create a new thread if the thread has locked due to time-out.