Part Number: BQ40Z50 Other Parts Discussed in Thread: BQ24610 , BQ24610EVM Hi guys,
How Can I connect BQ40Z50 with BQ24610 to charge or discharge battery 3S?
The AC/DC adapter input BQ24610 is 15V - 60W, and the setup cell pin is 3 cells. When I plug in…
Part Number: BQ24610EVM Below are the voltage measured by using digital multi-meter on respective pins of BQ24610-evm with external power applied.
VCC=12.15V
PG=0V.
REGN=6V
STAT 1 -3.4V
STAT 2-3.4V
VFB=.934V
CE-3.28V
ACDRV-7.2V
BATTDRV-9.28V
BATTERY WILL…
Part Number: BQ24610EVM Other Parts Discussed in Thread: BQ24610 I was wondering if th BQ24610 evm could be powered by DC power, if so which positions should the jumpers be in the correctly charge a battery?
Hello Pieter,
PieterT said: I essentially want to ensure that the BQ24610 will not struggle to supply peak currents from the batteries to the ublox module during data transmission. I am worried about how quickly the BQ24610 will be able to react when…
Part Number: BQ24610 Other Parts Discussed in Thread: , BQ25750 Hi TI,
I am designing a medical device, and I am considering using the BQ24610 charger. Is this part recommended for new designs?
The battery configuration is Li-ion 3S2P with 11.1V nominal…
Part Number: BQ27220 Other Parts Discussed in Thread: BQ24610 , , EV2400 , BQ25606 , BQSTUDIO , GPCCEDV , BQ27320 , BQ24610EVM Dear TI team,
I am currently working on a project that needs a Battery Charger and a Fuel Gauge for accurate Battery SoC tracking.…
Part Number: BQ24610 Good day,
I've previously had an issue with our BQ24610 charger burning and identified the problem as poor PCB layout (initial design was 2 layer PCB with single sided assembly) . I've redesigned our charger based on the BQ24610EVM…
Other Parts Discussed in Thread: BQ24610EVM Dear All,
One of my customer is planning to use BQ24610EVM directly in their end product, hence they would like to know dimensions of it. we are uable to get this information in web, we need your valuable help…