Part Number: BQ24616EVM Other Parts Discussed in Thread: BQ40Z50 , , BQ24616 Tool/software: Hello,
I have a 3S battery pack with a BQ40Z50 controller. This works fine. I am able to charge it with a commercial 3S charger - all good.
I now want…
Part Number: BQ24616EVM Other Parts Discussed in Thread: BQ40Z50 , BQ24616 Tool/software: I am designing a charger for a lithium ion battery pack of 3S using the chip BQ24616RGER I need to be able to isolate the AC charger adapter side to eliminate noise…
Part Number: BQ24616EVM Other Parts Discussed in Thread: BQ24616 , I am going to make a product using bq24616. I want to use bq24616evm without major deformation.
I am using Altium and would like to receive project data that is compatible with it. …
Part Number: BQ24616EVM Hi Team,
I encountered some problems while testing the 24610EVM board,
Cannot use electronic load and power supply to simulate battery
My input is a 24V power supply, and the BAT is connected to the electronic load CV mode…
Part Number: BQ24616EVM Hi, Good day. I hope you are doing well. Our customer is looking for the Altium design files for the BQ24616EVM. I would appreciate if you could help us provide the said files. Thank you and stay safe. Regards, Cedrick
Part Number: BQ24616EVM Other Parts Discussed in Thread: BQ24616 Will the BQ24616 take a DC input? The EVM states "AC adapter operating range"????
Thanks
Part Number: BQ24616EVM
Hi
I just purchase the BQ24616EVM and the unit is not charging and stat light is off.
* Vin is 20V-24V,
* Battery is 4 cell series 3.7V per cell. Vbat is set for 15.2V
* ACDRV , CE, PG Led is ON.
* No current is drawn…
Part Number: BQ24616EVM Other Parts Discussed in Thread: BQ24616 Below is my setup
Input voltage: 20V/4A or 24V/4A
Output voltage 12.6V
Observations:
Case #1: Only connect DC load to VSYS and GND (J5 pin 4 and 2): Can deliver 20V/4A or 24V…
Part Number: BQ24616EVM
Hi
We just purchase BQ24616EVM and we having issues when charging is almost done. The stat1 starts blinking and you can see on multimeter 2.5A coming on and off. The stat2 led never comes on to show the end of charging.
Our…
Part Number: BQ24616EVM Other Parts Discussed in Thread: BQ24616 Hi,
For the BQ24616EVM board, please refer to below picture whether i have configure correctly. As per below configure, my battery cannot
charging directly, is there any connection i…