Part Number: BQ24630 Hi Team,
The product page shows the max charge current is up to 10A. However, the datasheet only mentions 20uF capacitance for 3A to 4A charge current. Can you advise how to calculate for charge current greater than 4A (9A to be…
Part Number: BQ24630
I was given this modified schematic to make a simplified battery charger.
My design is not working yet and I have some questions.
What do I need to set ACSET to?
Can ACDRV and BATTDRV be floating?
Part Number: BQ24630 Other Parts Discussed in Thread: BQ24620 , Tool/software: I am designing a standalone battery charger for 8 LifePo4 6000mAH Cells in parallel. I do not need any other features. The BQ24620 does not work because the safety timer is…
Part Number: BQ24630 Tool/software: I have used this charger on a multiple other packs to charge a 3s 3p LiFePO pack. The circuit design is very similar to the datasheet shown below:
Only one pack seems to have this problem, but replacing the charger…
Part Number: BQ24630 Tool/software: Hi team,
We are trying to charge a 1500mAh 4S LiFePO4 battery using the BQ24630. When we apply 24V, whether the battery pack is connected or not, the Vref and Vregn voltages do not appear. The VCC voltage is 24V,…
Part Number: BQ24630 Tool/software: Hi,
From what i can see the device is behaving as it should but Im a bit confused with the STAT1 and STAT2 pins.
I have them connected to an MCU and to a LED shown in the image below. Ive noticed that it says LED…
Part Number: BQ24630 Other Parts Discussed in Thread: BQ76905 ,
Tool/software:
Dear all,
I would like to describe my issue:
I'm using the BQ24630 to charge a 4 - series cell (Lithium Werks 18650 1100mAh 30A LiFePO4), combined with a BQ76905 for…
Part Number: BQ24630 Tool/software: Hello,
I have trouble with the charging process of my design. I used the BQ24630 chip the schematic looks like this:
My charging curve is not as I expected continously. It stops after every 1min24sec and starts…
Part Number: BQ24630 Other Parts Discussed in Thread: BQ78350 , BQ76920 , Hi
The customer design with BQ24630 to charge BQ78350+BQ76920. They found it is easy to burn the BQ24630 and its peripheral components.
BQ76920+BQ78350 battery management board…
Part Number: BQ24630 Hi Team,
When charging is completed, there will be an abnormal state of charging and discharging flashing. Attached is the charge and discharge log. It includes the charge and discharge logs of normal machines and NG machines. …