Part Number: BQ24630 Other Parts Discussed in Thread: BQ25306
Hello TI experts,
my customer made PCB sample using BQ24630, there is some problems about charging time and constant current.
I show you some results below;
1. charging current is changed…
Use BQ24630 ,In accordance with the specification:
charge in progress:stat1 ON stat2 OFF
charge cmoplete:stat1 OFF stat2 ON
charge suspend,timer fault,over-vo1tage ,sleep -mode ,battery absent,stat1 OFF stat2 OFF
howoever,Start power charge…
Part Number: BQ24610 Other Parts Discussed in Thread: BQ24617 , BQ24616 , , BQ24618 , BQ24630
Please see the below document for the layout guidelines and example for the BQ24610, BQ24616, BQ24617, BQ24618, and BQ24630.
Layout Guidelines and Example…
Part Number: BQ24630 I am working with the BQ24630 for a LifePo4 charger, but want to charge the latest version of Lithium cells now, NMC.
Differences between LifePo4 and NMC:
LifePo4:
nominal voltage: 3.2V charging voltage: 3.65V
NMC:
nominal…
Part Number: BQ24630 Hi E2E Team,
my customer wants to use BQ24630 IC for only charging the battery, not for the adapter power to system.
In this reference design, we have 3 questions.
1. we will not use "SYSTEM" net on the top-right of the design…
Part Number: BQ76920 Other Parts Discussed in Thread: BQ24630 Hi Team,
For Lithium Iron Phosphate battery such as US26650FTC1A LFP/Gr from Murata, how do we connect BQ76920 and BQ24630 to multiple batteries?
Regards,
Danilo
Part Number: BQ24630 Other Parts Discussed in Thread: BQ24610 Or can someone suggest a better alternative? I have a 2s design for IS that requires higher than 8.4V charging voltage to account for diodes in the charge path.
With the 24630 I can program…
Part Number: BQ24630 Other Parts Discussed in Thread: BQ24620 , , BQ76930 Hi,
I'm looking into a solution to charge an 8S LiFePO4 battery pack. I came across the BQ24620 and BQ24630 components but they only support up to 7 cells in series. I could not…
Part Number: BQ24630 When BQ24630 in fully charged status, a pulse dischage performed(1s duration), VCC will equal to SRP for 1S, Will BQ24630 enter sleep mode in the 1s discharge duration? Then recovery the charge power followed the pulse discharge,…
Hi Kedar
Thanks a lot - this is the confirmation we needed.
Our test suggests 22uH / 10uF is stable throughougt BQ24630 charge cycle, so problem solved.
Great service from Texas Instrument.
Michael