Part Number: BQ24650 Dear Sir,
My BQ24560 circuit doesn't work, please help to review my schematic and share your comments. Or any guidance you can share with me that will be great! Thanks.
BRs
Henry
Hi Mike,
Thanks for the reply..
Yes, its do with the BMS module. All the voltages from BQ24650 were right and Charging Status LED's was 'ON' as well.
BMS needed a high current to wake it up. After BMS is awake, battery charging had no issues…
Part Number: BQ24650 Hi
The customer design with BQ24650, they design the charge current about 4A, but the actual current more than 5A.
They set the Vtopping is 14.7v, but the actual voltage mare than 15V.
Attached the schematic for your reference.
Please…
Part Number: BQ24650 Other Parts Discussed in Thread: BQ25798 Hi team, We are looking for an BQ that can control MPPT and satisfy the following specifications. *SPEC Input voltage for solar panel : 10V~23V Battery : Acid chemistries(13.6V/4Amax) If you need…
Part Number: BQ24650 Hi team,
Could you review my design, please? See below the conditions and the file with the design.
Solar Panel 21V, battery Li-ion 1-cell, ICHARGE = 4 A, IPRECHARGE = 0.4 A
/cfs-file/__key/communityserver-discussions-components…
Part Number: BQ24650 Other Parts Discussed in Thread: BQ40Z50-R2 , Hi, I am working with 2S5P battery pack I chose to work with the BQ40Z50-R2 gauge and the BQ24650 to charge the battery pack. My problem is that the CHG won't work. I checked the voltages…
Part Number: BQ24650 I have got problems with the charger circuit. This will only charge at 145mA max and both status LEDs are on that indicates a fault. At the moment I have been on this hours and not getting anywhere. I have established the following…
Part Number: BQ24650 Hi Team,
Can BQ24650 work with 28V ± 2% supply voltage (the supply voltage comes from an AC-DC module)?
Assuming BQ24650 work with 28.56V Vin, whether its reliability will be reduced? If yes, what is the true maximum continuous…
Part Number: BQ24650 Hi Team,
The battery charge voltage (Max) of BQ24650 is 26V, and usually lead-acid battery single-cell voltage is 2V, it seems that a maximum of 10+ cells can be connected. So, why is BQ24650 limited to connect only 1~6 cells?
Best…