Part Number: BQ24735EVM-710 Hi Sir/Madam,
We are selected one of the battery in our design, battery is comprised of seven (7) Lithium Ion rechargeable 21700 cells, assembled in a 7 series / 1 parallel (7s1p) design.
so, We need to know which charger…
Part Number: BQ24735EVM-710 Are the schematics and PCB files (Supported in Altium or Kicad) available for the following EVM:
BQ24735EVM-710
Please let me know because i need it for my reference only.
Thanks for your help with this!
Part Number: BQ24735EVM-710 Other Parts Discussed in Thread: EV2400 , , BQSTUDIO , BQ24735 , BQ24800 , BQ24780S I'm trying to use the BQ24735EVM-710. I've bought the evaluation board and also MSP430 Controller EV2400. Also, I've installed TI's Battery…
Part Number: BQ24735EVM-710 Other Parts Discussed in Thread: BQSTUDIO , BQ24735 , EV2400 Tool/software: Code Composer Studio Hi,
Please read the test report below.
Through the analysis of I2C waveform by oscilloscope, interference ripple is found…
Part Number: BQ24735EVM-710
What could be the cause of the Q1 MOSFET failure, the Gate shorted to the Drain, on the development board? I am running the board from a 24V power supply.
Part Number: BQ24735EVM-710 Other Parts Discussed in Thread: BQ24735 The listed input range max for this EVM design is 24V, yet it appears that this will exceed the Recommended Operating Conditions Max of 22V.
The device max is 30V with 24V listed as…
Part Number: BQ24735EVM-710 Hello E2E,
I got the BQ24735EVM-71, and I test it. The EVM is setted ILIM=4A. I inputted 0x0200 to 0x14 register. However, charging current was 4A, the inputted number was ignored. Please let me know the reason.
Best regards…
Part Number: BQ24735EVM-710 Other Parts Discussed in Thread: EV2400 Hallo,
I am using the BQ24735EVM-710 Evaluation Module, but when I presse the ''read'' button of the Evaluation Software, it always says''error''.
I use EV2300 to communication, and…
Part Number: BQ24735EVM-710 Other Parts Discussed in Thread: BQ24725AEVM-710 There is a forum post on this topic, but the engineer that asked the customer to email them does not seem to be with the company anymore. So I am going to post this again.
…
Other Parts Discussed in Thread: BQ24735 Dear support team,
Now I am using a MCU to connect with your board( BQ24735EVM-710 ) by I2C.
Set up on My Board:
J1: connect to 22V
J2(BAT-GND): connect to my battery
SDA: connect to SDA of MCU
SCL…