Other Parts Discussed in Thread: BQ24753A , BQ24753 Dear e2e,
In a setup with a 15V power net DC supply and a 12.6V Accu pack, we use the BQ24753A with a ACSET Limit 2A (via resistor divider) and configured also the SRSET Limit via a resistor divider to…
Hi,
The main differences is on the Temperature monitoring (bq24753 does not have one) and the OVP protection (bq24753 is programmable). Please read the application Note (SLUA498) for more details about the differences between bq24750A and bq24753…
Other Parts Discussed in Thread: BQ24753 Charge current is set to 400 mA.
At Vcc of 14V, charge current is stable at 400 mA.
When Vcc increases to 16V, charge current drops to 280 mA.
I'm read the datasheets, and re-reading the datasheets but it's still…
Other Parts Discussed in Thread: BQ24753 , BQ24620 , BQ24630 , BQ24650 , BQ24610 Hi guys ,
I need a battery charge for lead acid and LiFePO4 ( 12V x 40 Ah ) where would you replace a battery for the other , was thinking of using the BQ24753 controller.
I…
The bq24753 must be told by the system host to terminate the charging.
bq2461x charger is stand alone charger. It can terminate the charge when the battery is fully charged.
bq24750A doesn't support the pre-charge function. But, bq24751B and bq24753 provide the pre-charge function when the battery voltage lower than the V BAT_SHORT threshold.
There is a comparison table for those devices. http://www.ti.com/litv/pdf/s…
bq24753 doesn't have a termination function. So, I call it a host control version. It means that the termination function is relied on the host controller. If a host controller can not detect the termination current or read the current out from the…
Other Parts Discussed in Thread: BQ24753 , UC3906 , BQ2031 Hello,
I want to build a charger for a VRLA battery based on a bq24753 and a PSoC.
I read the bq24753 datasheet and I don't find how I can set the charge voltage to the requirements of my battery…
Other Parts Discussed in Thread: BQ24751B , BQ24753 , BQ24105 , BQ24745 , BQ2954 I am trying to build a charger for mine 3 cells LiFePO4 and got BQ24753 and BQ24751B sample. I am a bit confuse where to get the host DAC for this chip.
For the Voltage and Current…