Part Number: BQ24800 Other Parts Discussed in Thread: BQ25758 , BQ25750
Hi Team,
May I check if our BQ24800 can hold 240W application? what is the maximum charge current of BQ24800? Can our BQ24800 support 20V12A application?
Best Regards,
Jaden Yue …
Part Number: BQ24800 Other Parts Discussed in Thread: BQ24161 Hi Representative.
Is it possible to make the BQ24800 work standalone like the BQ24161? Does the BQ24800 have a charge timer function? I want to use the BQ24800 to charge 18650 batteries
Regards…
Part Number: BQ24800 Hi
Could you help to suggest suitable Buck Boost Charger IC conditions as follows
1. 32V Input Voltage Max, 9V Min
2. 3 string batteries, 12.6V charging voltage.
3. 3A charging current.
4. Support IMVP PROCHOT function.
5. SMB…
Part Number: BQ24800 Hi All,
I have a question about BQ24800.
Does BQ24800 have a Li-ion charging profile? Also, are charging profiles provided when controlling with an external microcontroller?
Best Regards, Ishiwata
Hi Svenn,
I will close out this thread since I have not received an update.
Feel free to open a new thread if you have further questions.
Best Regards,
Aya Khedr
Part Number: BQ24800 While implementing the BQ24800 I noticed that according to the datasheet, the nPROCHOT pin should be connected through a 500 ohm resistor to the 1.05 V voltage rail. Later in the example schematics, we can see that the pin is connected…
Just to make my question clearer, the bq40z50-r1 has a charging voltage and charging current regiater that can be broadcasted to a smart charger. Checking the registers of bq24800, the same register can be written. Im thinking if it is possible for the…
Part Number: BQ24800 Hi Expert,
My customer want to know what is the propose for the watchdog feature? And how do I know if the bq24800 trigger watchdog function? Any register will indicate it?
Far
Part Number: BQ24800 Other Parts Discussed in Thread: BQ25756 Dear all,
Would it be possible to use BQ24800 to replace LTC3350 for supercap management?
Here you can find more details about the application we are interested to:
input voltage: 12V
Supercap…