Part Number: BQ25050 Hi,
In our design there is no TS pin for the battery we are using, so we connected a 47 kohm resistor between TS pin of charger IC (BQ25050) and ground. The battery is charging with no issue since, but we observed that the /CHG…
Part Number: BQ25050 Hi everyone,
We are using a BQ25050 charger in our product. It works great, but we are adding a testing step in our production where we want to measure the system power draw after assembly. The system consumes in the range of 100uA…
Part Number: BQ25050 Hi Sir
From DS "TYPICAL APPLICATION CIRCUIT",
May BQ25050 /CHG pin can removed 100K pull up resistor if our HOST internal site GPIO pin have 13koohm resistor pull up to VGPIO=3V?
bogey
Other Parts Discussed in Thread: BQ25050 Hi,
My design includes BQ25050 and a LiIon 1 cell battery.
When the battery is not charging but is used to deliver power for the system in run time, I am wondering how much power BQ25050 is consuming.
In…
Other Parts Discussed in Thread: BQ25050 We use the BQ25050 to charge our battery, but during fab tests we need to power the board with no battery plugged.
When we try to power up the system in this configuration we see 4v on the OUT pin with low gliches…
Other Parts Discussed in Thread: BQ25050 , BQ25060 , BQ24070 I've got a couple questions around the BQ25050/BQ25060 parts.
I am unclear as to the operation on "OUT". From the datasheet I can see that it will be greater than 3.4V when there is an input…
Other Parts Discussed in Thread: BQ25050 Dear all,
I have the EVM of BQ25050/25060 on hand.
Test environment: EVM of BQ25050/25060. The adapter output voltage is 5.3V 2A, the battery is under 3.8V, the load is electronic load (in CC mode).
According…
Part Number: BQ25050EVM Other Parts Discussed in Thread: BQ25050 I just recently purchased an BQ25050 EVM to evaluate for use in our application. When following the users guide after connecting the main power in step 4.1.1 and then measuring the LDO there…