Part Number: BQ25060 I am redesigning a small wireless device that uses a 240mAh Li-polymer battery pack with no thermistor. I want to replace the existing charger IC with the bq25060.
What is the best way to "disable" the NTC monitoring? I assume just…
Part Number: BQ25060 Hi Sir,
If the EN pin is connect to ground the resistor connected to Iset will control the input current.
If i set the input current to 177mA. VIN has connected to USB.
When the output current is around 550mA, the charger IC will…
Part Number: BQ25060 Hi Sir,
Could you help to review the schematic as attachment? Is there any suggestion?
Other questions need to your support as below:
1.If the temperature over 45°C, then back to normal temperature. What is the safety timer for BQ25060…
Part Number: BQ25060 Other Parts Discussed in Thread: BQ24040 , , BQ24074 Hi, team, The following is described on page 12 of the data sheet. I have some questions about this description. Please tell me about them.
=== Description on Datasheet_Page-12 ==…
Part Number: BQ25060 Other Parts Discussed in Thread: BQ24072 Hi
If the EN pin is connect to ground the resistor connected to Iset will control the input current.
Is it possible to keep the input current set to 1A, but change the max charging current…
Part Number: BQ25060 While being initially connected to BAT only at POWER ON stage, does the bq25060 needs to have external source at IN to allow the battery powering system load?
Part Number: BQ25060 Other Parts Discussed in Thread: BQ24296 Hi,
i need to design a system where normally i have dc power connected to it and only when its removed, i need to use back up battery.
Other limitation comes from temperatures. Battery can…
Hello Kevin,
There are a few issues that I see here.
First what sort of battery are you using and is it really only 3V? That on top of the fact that you system has a max voltage of 3.9V.
The bq25060 is set to regulate the battery voltage during charging…
Part Number: BQ25060 Hi team,
we are working with a ctm experiencing some issues while using our BQ25060.
They’re using it in a project under evaluation/characterization. Here below ctm comments :
“.. BQ25060 stays in a system using a primary…