Hi Jim,
user4839477 said: Is the USB500 standard 500 milliamps of input current?
Yes, USB500 refers to an input current limit of 500mA.
user4839477 said: Is there an easy way of disabling the TS monitoring. I have followed the datasheet with 490…
Nick, having difficulty uploading the pdf. The issue centers around the output of the solar harvester SPV1040 (ST Micro). It does not provide a well regulated voltage to the BQ25071. When the input voltage to the BQ25071 drops below threshold, the LDO…
Part Number: BQ25071 Other Parts Discussed in Thread: BQ24105 Dear team,
Customer are looking for battery charger solution for Coin type lithium battery - ML2020.
Did we have charger solution for this battery? The normal battery voltage is 3V. …
Part Number: BQ25071 Hi Team, There's no SPICE model available for BQ25071 in the TI website. Our customer is requesting to have its SPICE MODEL. Can you share it here if it is possible? Thanks! Jonathan
Part Number: BQ25071 I'm looking for small PCB footprint solutions to charge a 45mAh LFP battery for a wearable device.
BQ25071 looks suitable except the datasheet specifies a minimum current of 100mA, but doesn't go into any detail about where that…
Part Number: BQ25071 Other Parts Discussed in Thread: BQ24650 , Hello,
We are evaluating using either the BQ25071 or BQ24650 for Solar Charging a LiFePO4 battery: The questions are related to the BQ25071. We see that the BQ25071 is simpler and optimized…
Hello
The LiFePO4 charge profile bq25071 -Q1 will use is constant current fast charge until battery voltage reaches VBAT(OVCH), 3.7V typical then terminates charge. After that point the bq25071-Q1 enters Float-Voltage Regulation Phase and output voltage…
Part Number: BQ25071-Q1 Other Parts Discussed in Thread: LM4041-N 1 I plan to go up the clipping voltage 3.5V to 5V of BQ25071-Q1
I'm going to insert 1.5 V zener diode between Out pin and BAT pin. Does this work? 2 According to the Block Dia. in the…