Part Number: BQ25071-Q1 Other Parts Discussed in Thread: BQ25071
Hi
I have two questions on the LifePo4 precharge current :
-What is the real voltage value (min / typ / max) considered in the BQ25071 for the precharge current for LiFePo4?
-What…
Part Number: BQ25071 Tool/software: WEBENCH® Design Tools Hi,
I wonder if there are any plans to release a WEBENCH model for the bq25071 LiFePO4 linear charger?
Thanks in advance,
Gustaf
Part Number: BQ25071 Hello,
I am working with the bq25071 and the datasheet gives the package dimensions but not the land pattern recommendations.
The TI Package Database also does not provide a recommended land pattern for this device package which…
Part Number: BQ25071-Q1 Hello,
Looking on the bq25071-Q1, I have a LiFePo4 3300mAH Battery 3.2V with cahrging float at 3.6V, also I have system load of 340mA
I was wondering if I set ISET for 1000mA Charging and leave it set as this, what will happen…
Part Number: BQ27Z746 Other Parts Discussed in Thread: BQ25071 Tool/software: We have download a new Golden Image from the CPU, will bq27z746 use the new settings without any command or do do we need to send a reset command?
We have big problem with…
Hi,
I think that a Co-based charge profile and the charge profiles of LiFePO4 are different. Please refer to a profile of bq25071. When the big difference is if arrives at voltage peak (OVCH), it stop CC and a point waiting to become VOUT(REG). In the…
Part Number: BQ25070 Other Parts Discussed in Thread: BQ25071 , BQ24210 The datasheet for the BQ25070 briefly mentions Vin-DPM which I believe would make it suitable as a solar charger for LiFePO4 single cells.
Can you confirm the suitability of the…