Part Number: BQ25100
Hello,
Customer wants to use 230mAh battery without NTC thermistor.
And wants to make enable and disable function by using TS pin.
Can BQ25100 be enabled and disabled by TS pin?
If possible, could you let me know how can make it…
Part Number: BQ25100 Other Parts Discussed in Thread: BQ25155 Hi team,
My customer has a couple of questions about the BQ2510x series. Can you help them out?
Charging current
At the beginning of the data sheet it is described that the charge controller…
Hi Bill,
Bill Johns said: This is a two IC solution BQ51003 + BQ25100, the battery charger can be replaced with BQ25170 that will work better at low charge currents.
This is good information! Since the BQ51003 complies with Qi, the frequency will be higher…
Part Number: BQ25100 I'm using the BQ25100 as a lithium battery changer and also as to provide power to the design. There are times when a lithium cell will not be needed. So how do I make sure the BQ25100 voltage out remains with in range with or without…
Other Parts Discussed in Thread: BQ25100 , BQ24040 , BQ21040 Is it possible to parallel two BQ25100’s? I need 350mA maximum charge current.
Even two in parallel would have the lowest of-state battery discharge current I can find. (With the charger…
Part Number: BQ27220 Other Parts Discussed in Thread: BQ25100 , Hello,
The title says it all, can I combine the BQ25100 (LiPo Single Cell Charger) with the BQ27220 (Fuel Gauge)?
My goal is to (re)charge a LiPo-Battery and allow the user to monitor / see…
Part Number: BQ25100 Other Parts Discussed in Thread: BQ24040 , During TTDM, CHG pin is high impedance.
After that, does CHG pin become low when battery is detected and charge cycle begins?
And also, does CHG pin become low when re-charge begins if OUT…
Part Number: BQ25100 Dear TI Sir
BQ25100 charge current = 10mA.
What's value of optional RC is better for charge current = 10mA.
R216 = 2.7K ; C = 10nF ( from SPEC. 9.1 Application Information )
Is it all right ?
Part Number: BQ25100 Hello,
Customer is designing their device with BQ25100.
She wants to change charging current during operation.
If she change Riset value during BQ25100 is operating, Can charge current be changed?
Or how she can change charge current…