Part Number: BQ25100 Hello,
Customer is designing their device with BQ25100.
She wants to change charging current during operation.
If she change Riset value during BQ25100 is operating, Can charge current be changed?
Or how she can change charge…
Other Parts Discussed in Thread: BQ25100 , BQ24040 , BQ21040 Is it possible to parallel two BQ25100’s? I need 350mA maximum charge current.
Even two in parallel would have the lowest of-state battery discharge current I can find. (With the charger still…
Part Number: BQ25100 Other Parts Discussed in Thread: BQ25101
Team,
PRE-TERM can be left floating so that the current is set to the default one given in the BQ25100 datasheet (SLUSBV8C page 6 - see below picture). Those min/Typ/Max specs are given…
Hello
Your system will load will be connected to the bq25100 output and battery, current out will be both current to battery and current system.
For the bq25100 to complete charge it is expecting the output voltage to reach 4.2V and then output current…
Part Number: BQ25100 Hi,
The minimum charging current of BQ25100 is 10mA. customer checked if we have solution to support the charing current lower than 10mA. the smaller ,the better. thanks.
Part Number: BQ25100 Other Parts Discussed in Thread: BQ24040
Dear All
Im designing a PCIexpress Motherboard For an important Factory Automation Project with xchangeable SoMs (Also Designed By Myself) Im using BQ25100YFPR For MotherBoard LiR2032 charging…
Haresh,
BQ25100 is a good choice for charging. If you need powerpath to support system load, you might consider BQ24232H.
If you need additional rails for a DC-DC or LDO and I2C programmability, you might consider BQ25120.
regards,
Gautha…
Part Number: BQ25100 Dear Experts
My customer need to order BQ25100L but I cannot find this part number in the website.
Could you let me know how to order it?
Thank you.
Other Parts Discussed in Thread: BQ25100 , BQ25100EVM-654 Hello,
I am using the BQ25100 in a wireless charging application. I'm using a 10k NTC on the TS pin. While charging, I'm picking up the wireless charger frequency on the TS pin which is causing…