Part Number: BQ25101
Hey Expert,
when VSYS=3.3V does the charge current will below 20mA? R508=13.5k ohm. so I fast charge=10ma
I saw the V lowv=2.4~2.6. on datasheet. so I will say no. when Vsys=3.3 still in fast charge right?
Thanks for your support…
Part Number: BQ25101 Hola,
Usamos BQ25101YFPR y encontramos un problema para la siguiente condición.
1. El PCM de la batería está habilitado por un voltaje de batería muy bajo.
Sin embargo, el PCM de la batería no se puede…
Part Number: BQ25101 Hi
The customer has a question about the status of CHG, Please help answer.
Case 1: Supply the load first, then VIN. During charging, CHG will be low, which is normal.
Case 2: Supply VIN first, then load, and during charging, CHG…
Hello Hao,
Sorry for the delayed response.
I was able to see identical behavior in case 2 & 3 with bq25101, using 5V supply on IN and battery simulator at 3.6V on OUT. I altered the TS voltage with potentiometer.
Hao Wang14 said: 2. When TS voltage…
Part Number: BQ25101 Other Parts Discussed in Thread: BQ25155 , BQ25150
We are using BQ25101 in our design. We implemented the same circuit given in the datasheet as below in the previous version of the PCB, but we had an issue. We couldn't bring…
Part Number: BQ25101 I want to monitor the charge current with an external ADC using the ISET pin. But I cannot find information on the ISET voltage range in the datasheet. What is the possible range of voltages on the ISET pin, and how would one convert…
Part Number: BQ25100 Other Parts Discussed in Thread: BQ25101 , , BQ25180 Tool/software: Hi Team,
Our customer "Mesi Medical" is working on a thermometer module where on the power side they are using
BQ25100HYFPR charger for battery.
BQ27427YZF…
Part Number: BQ25101 The nCHG behaves as expected when the battery, being charged, is disconnected from the load. However, when the battery is connected to a very small load (> 100uA), the nCHG stays low way beyond the 1.5mA termination current (I have…
Part Number: BQ25101 Other Parts Discussed in Thread: BQ25100 I was originally planning on using the BQ25100, but want to swtich to the BQ25101.
cannot find any information concerning the pre-charge_current/fast-charge_current and termination_current…