Hi Ronit,
What happens if you lower the TS voltage to a normal range? It looks like you are in TTDM now. It could be possible that you hit the safety timer. What is the CHG/ pin doing right now?
Regards,
Mike Emanuel
Part Number: BQ25101H Team,
What is the meaning of the below parameter? Vout (max) with BQ25101H is defined 4.35V. What is the meaning of that 4.40V?
Thanks in advance!
A,
Part Number: BQ25101H Hi Team,
I want learn more about the function of external RC circuit when charging current is small, why we need the external RC and how it works. DS mentioned for a more stable current, but it is not clear enough to me.
And if…
Part Number: BQ25101H Dear Support,
My customer is facing some issue to detect the end of charge with our bq25101H, for small charge current (at 20mA). The RC network is well placed, on Iset. The test has been done for higher charger currents and the…
Part Number: BQ25101H Other Parts Discussed in Thread: BQ25101 Regarding battery charger BQ25101H, I have been measuring an efficiency of ~80% at a load of 3.7V, 100mA. I was expecting a higher efficiency of this part, I am planning to test the EVM this…
Part Number: BQ25100 Other Parts Discussed in Thread: , BQ25101H , Hi
I want to know why the BQ25100A can normally work between -40°C to 85°C,But the BQ25100,BQ25101H, BQ25100H 'S Op Temperature is from 0°C to 120°.Isn't this temperature range very unscientific…
Part Number: BQ25101H Other Parts Discussed in Thread: BQ25101 Hello,
bq25101H has no PRE-TERM pin, What are pre-charge and terminate level for bq25101H ? Thank you.
BR
Patrick
Part Number: BQ25101H Other Parts Discussed in Thread: TPS62743 Dear e2e Community,
One of my customer has the following issue with our BQ25101H charger:
When they try to use a battery which is mostly charged (~ >4.1V), the /CHG pin stays at '0' (in…
Other Parts Discussed in Thread: BQ25101H Hi Ti Team,
This is Rajesh from Happiest Minds.
We are using BQ25101H in one of our designs.
Without battery connected we would get 4.2V regulated output and 22mA of initial output current .
Does the charger remain…
Other Parts Discussed in Thread: BQ25101H , BQ25101 Hello, I am using the Bq25101H to charge at a max rate of 36mA. Everything works as it should except the !CHRG pin doesn't go low when the battery current drops below 10% in the voltage regulation and…