Part Number: BQ25155 Operation has been confirmed using BQ25155EVM. The app used is "Battery Management Studio". I would like to perform a charging operation, but the charging current does not flow. The current flowing to VIN5.0V is 10mA or less. There…
Part Number: BQ25155
Operation has been confirmed using BQ25155EVM. The app used is "Battery Management Studio". I would like to perform a charging operation, but the charging current does not flow. The current flowing to VIN5.0V is 10mA or less. There…
Part Number: BQ25155 Other Parts Discussed in Thread: EV2400 , , BQ25150 We have started considering evaluation boards. It seems like the assumption is that VDD output = VIO input is used as the default. Personally, I tried connecting it to use VLDO output…
Part Number: BQ25155EVM Other Parts Discussed in Thread: BQSTUDIO , USB2ANY , , EV2400 , BQ25790 Can the USB2Any be used with BQStudio? I have the USB2ANY from a previous evaluation board. I'm testing with the BQ25155EVM, but it only seems to work with…
Part Number: BQ25155EVM I've removed J4 (extra 3.3V header) from the board and connected J7 (VBAT header) to a Keythley 2450 SourceMeter. The board preforms as expected with ~800nA being consumed from VBAT while PMID is also outputting the same voltage…
Part Number: BQ25155EVM Other Parts Discussed in Thread: BQ25155 Hi,
I have questions about some watchdog defined for the device BQ25155.
In the chapter 8.3.2.2 Safety Timer and I 2C Watchdog Timer of the document bq25155.pdf , this is reported…
Part Number: BQ25155EVM Other Parts Discussed in Thread: BQ25155 Hi,
Condition: device in Low power Mode, V IN < V UVLO , V BAT > V BATUVLO so the battery discharge FET is turned on connecting PMID to the battery.
Event: V BAT < V BATUVLO
After…
Part Number: BQ25150 Other Parts Discussed in Thread: BQ25155EVM , BQ25155 We are using BQ25150 in one of our boards
We are facing issue with the values of two registers in the IC
Content on reset as per the Datasheet ICHG_CTRL (Address = 0x13) [reset…
Part Number: BQ25155 Other Parts Discussed in Thread: EV2400 , Hi, I am currently trying to use/implement driver of the BQ25155 LDO/Charger and I am facing problem and having some questions. I am using BQ25155EVM/Battery Management Studio with EV2400…