Part Number: BQ25170 Other Parts Discussed in Thread: TPS62808
Hello, I am using the BQ25170 to charge a 4.2V 1 cell Lipo battery. I have ordered 5 PCB’s and only 1 out of 5 charges my battery from 0V (When the voltage is cut off from the PCM). …
Part Number: BQ25170 Other Parts Discussed in Thread: TPS63070 , , BQ24170 , BQ25798 Tool/software: Hi teams,
I have a portable application that is evaluating the TI's solutions.
I draw a simple block diagram as below, could you please suggest the…
Part Number: BQ25170 Other Parts Discussed in Thread: BQ27220 Tool/software: Hi
I have used BQ27220 and BQ25170JDSGR for fuel guage and charger IC respectively in my system. I have connected BIN pin and TS pin of BQ27220 and BQ25170 IC respectively…
Part Number: BQ25170 Hi, I'm trying to charge a 3.7V lithium coin cell and I have the below circuit. I'm measuing 5.0V on the input of the charger and I have the battery voltage on the output but its not charging and the supply current is jumping up and…
Part Number: BQ25170 we are using BQ25170DSGR for charging 4.2V LiPo Pouch cell.
STAT is pulled up by 10k and connected to GPIO. when the charging is enabled, STAT pin is pulled low after 2 sec and not immediately.
is it normal operation ?
what…
Part Number: BQ25170 Other Parts Discussed in Thread: BQ25180 , BQ24133 , BQ25185 , TPS63020 , TPS63060 , TPS63070 Tool/software: Hi, I need help in selecting a lipo battery charger. I have micro hydro generator with the following specs.
DC5V Technical…
Part Number: BQ25170 I am using BQ25170 to charge Li-Ion battery of 4.2V with 200mA charging current.Input is 5V from USBC
For setting the 200mA i will set the RISET to 1.5k. (RISET=300ohm*A/200mA).
During CC mode current will be 200mA,during trickle…