Part Number: BQ25170 Tool/software: Hi,
I designed a charger with a digital potentiometer connected to the VSET pin. The datasheet provides a table with discrete resistance and end charge voltage values.
The voltage variation with the resistance is…
Part Number: BQ25170 Tool/software: Hi team,
In related thread , below are described.
The charge disable function of the TS pin provides a means to turn off automatic recharge, which is part of the charging profile by default.
System will need to have…
Part Number: BQ25170 Tool/software: I am trying to protect a lithium battery from an over voltage and over current when single fault failures occur on the battery charger. If ISET on the BQ25170 is shorted, the current to the battery will exceed the…
Part Number: BQ25170 Tool/software: I have a design for BQ25170 that is almost identical to the application note for charging a single cell Li-po battery but when supplied with 5V for VIN the chip appears to turn on and off at a period of around 2 seconds…
Part Number: BQ25170 I was able to run the BQ25170 through a couple of charge/discharge cycles and it was working. We need to get CSA approval and one of the tests they will run is short IN to OUT and confirm the charger stops charging. So, I did that…
Part Number: BQ25170 Tool/software: Hello,
Is it possible to share the battery thermistor (NTC) between the BQ25170 battery charger IC and a fuel gauge (MAX17262)?
Thank you in advance.
Best regards,
João Rego