Part Number: BQ25171-Q1 Tool/software: Hi All
We are used a BQ25171-Q1 to charge a LIPO with the Ilimit set to 200mA (1.5K), Vset 4.1V (24K) timeout 5hrs (100K) and no temperature measure (10K).
The charger sequence behaves as expected and fast charges…
Part Number: BQ25171-Q1 Tool/software:
"OUT overvoltage falling threshold, per cell for NiMH chemistry".
How can I understand the falling threshold? It means in discharge status? but it is charger protection.
Part Number: BQ25171-Q1 Tool/software: Hello support team,
I have made the BQ25171-Q1 charger followed exactly the sample schematic on datasheet, it will charge single cell LiFePO4 battery with 400mA current. The Vset resistor then is 82K (3.6V according…
Part Number: BQ25171-Q1 Tool/software: We were looking at the data sheet for the subject charger IC, specifically the ISET fault conditions. In section 7.4.4 of the data sheet the nonrecoverable ISET condition states pin short detected, while Table 7…
Part Number: BQ25171-Q1 Tool/software: HI TI,
For a 3S NiMH config, how does the BQ25171 judge the battery is full ? It there any voltage thershold of a full 3S NiMH battery package? Or the Constant charging will keep going until the Charge Timer(16h…
Part Number: BQ25171-Q1 Tool/software: Hi Team,
I am requiring some assistance in selecting the best suited product for a particular application which may stray a little from general use cases. The device is to be fitted into a car, and the idea is that…
Part Number: BQ25171-Q1 Tool/software: Hello, is it possible to use load sharing with BQ25171-Q1 ? I'd like to have use USB 5V power and battery power.
When 5V USB power is connected it should power the load and charge the 3.6v NimH battery. In that…
Part Number: BQ25171-Q1 Other Parts Discussed in Thread: BQ25170 , BQ25172 , Tool/software: Hi support team,
Are there plans to release a non-Q1 version of BQ25171?
Regards, Dice-K
Part Number: BQ25171-Q1 Hi Team,
The Query is regarding BQ25171-Q1 Charger IC.
From Data sheet, Fast charge timer can be set to 5 hr and 10 hr only for Li+ battery.
is there any impact in charging cycle if the battery get fully charged and charge cycle…