Part Number: BQ25171EVM Hello Team,
Good day. My customer is requesting the Gerber files of our EVM BQ25171EVM. They will use the EVM as bases of their project,
Regards,
Renan
Hello
See below from the EVM User's Guide.
Shorting Jumper on JP6 should be in the Fixed position, this will connect 10k to the TS pin (Pin 4) and provide a safe condition.
user4863518 said: 10kΩ between TS4 and GND when shipped?
Yes -- will be 10k…
Part Number: BQ25171EVM Other Parts Discussed in Thread: BQ25171-Q1 I have built a development board referring to the NiMH rechargeable battery circuit on page 3 of the application note BQ25171-Q1 Quick Start Guide, and STAT1 and STAT2 show the waveforms…
Hello Nick,
Thank you very much for your answer! I have some additional questions.
As I understand from your answer: «As long as you are staying under the max rating on the /CE pin you are OK ( 5.5V) . The /CE pin is connected to an input of comparator…