Part Number: BQ25172 Tool/software: We are using the BQ25172 to intermittently charge a 4-cell NiMH battery pack for 12 hours at 120mA. The VBAT status is connected to an LED and an input to a microprocessor (which is configured as an input), the STATUS…
Part Number: BQ25172 Tool/software: Hi team,
Are the resistors connected to the TMR pin limited to those listed in Table 7-1? For example, is it not possible to set the charging time to 5 hours?
Best Regards, Ryu.
Part Number: BQ25172 Other Parts Discussed in Thread: BQ2002 Tool/software: Hi team,
Since the BQ25172 uses a timer-based charging method, we believe there may be concerns about overcharging. Given that the minimum safety timer duration is 4 hours,…
Part Number: BQ25172 Other Parts Discussed in Thread: BQ25176 Tool/software: Hi Team,
Please provide BQ25172 OVP rising & falling test waveform or timing diagram
Thanks
Part Number: BQ25172 Tool/software: Hi TI team,
We are currently designing a circuit using the BQ25172, and would appreciate your help reviewing our schematic to ensure there are no obvious mistakes or issues.
Thanks!
Part Number: BQ25172 Other Parts Discussed in Thread: BQ24105 , BQ25710 , BQ24810 Tool/software: Hi Sir,
My customer is seeking a NiMH battery management IC that supports 9V input, 1.5A charging current, series two NiMH cells, and the top-off charge…
Part Number: BQ25172 Tool/software: Overcharging will affect battery life. NiMH battery suppliers recommend that overcharging be defined as charging above 1.5V. BQ25172 datasheet: Vout_OVP: 1.7V. Does TI have any other suggestions for this part?
Part Number: BQ25172 Tool/software: Hi team,
Customer plan to use NiMH in their design, their NiMH voltage is 1.3V, and plan to use 2-cell in series.
BQ25172 voltage is 1.7V, this is larger than their battery voltage.
Could you help check if we…
Part Number: BQ25172 Tool/software:
We are testing the BQ25172 linear NiMH Battery Charger on our new product in development. From our findings, when we set up a 1-Cell NiMH battery as the device to be charged and the BQ25172 (VSET) is set to '1-Cell…
Part Number: BQ25172 Other Parts Discussed in Thread: BQ25505 , BQ25750 Tool/software: Can BQ25505 and BQ25750 support nickel-metal hydride batteries (NiMH)? If not, what problems will occur when used with NiMH batteries? For BQ25172 used with NiMH, is…