Part Number: BQ25180 Hello,
We are using BQ25180 in wearable device. We are facing an issue when the battery is deep discharge. Below is register configuration,
[0x03] VBAT_CTRL = 0x46 [0x04] ICHG_CTRL = 0x25 [0x05] CHGCTRL0 = 0x24 [0x06] CHGCTRL1…
Part Number: BQ25180 Hello,
Could you please clarify the actual purpose of the Input Current Limit Protection (ILIM) in the BQ25180? We would like to confirm which current path this limit is applied to. Thank you for your support.
Part Number: BQ25180 Other Parts Discussed in Thread: BQ25188 Hello, I would like to request the current lifecycle status of the BQ25180 to understand if its recomended for new designs? our device is an industrial product with a lifecycle of 10 years…
Part Number: BQ25180 Other Parts Discussed in Thread: , BQ25188 Hello TI
I am struggling with a voltage ripple on the SYS output voltage. This ripple voltage only occurs under a certain condition. SYS supplies my electronics, on BAT there is a rechargeable…
Part Number: BQ25180 Hi, the BQ25185E datasheet specifies a pull-up resistance range of 1 kOhm to 20 kOhm.
Would there be any issue if I connected these pins directly to my MCU GPIOs, which have internal weak pull-ups with a maximum resistance of 50…
Part Number: BQ25180 Other Parts Discussed in Thread: BQ25188 , BQ25185 Tool/software: Hello,
Considering the need to programm the bq25180 by I2C bus. I understand that any time the device is reset it must be programmed by the controller. Is this right…
Part Number: BQ25180 Hello,
Is it possible to share a single battery NTC between a charger IC and a fuel gauge?
I’d like both devices to use the same temperature reference, but I’m concerned that since these inputs may source current for NTC measurement…
Part Number: BQ25185 Other Parts Discussed in Thread: BQ25180 , TPS631000 , BQ25188 , BQ25606 Hello TI Team,
I am currently working on a power design and would appreciate your guidance and support.
Below are the design details:
Input Supply: 5V…
Part Number: BQ25180 We are using BQ25180 to manage a small backup battery in a product. During manufacture we set the battery to a low power mode to minimise cell discharge in transit.
We know we have the option to use Ship mode with a slightly higher…
Part Number: BQ25180 Other Parts Discussed in Thread: BQ27427 Hi Team,
We use the BQ25180 and we find there are two different C2 pin voltage if we used USB to power up. (We didn't connect the battery) Some are 4V and some are 2V. We need 4V to release…