Part Number: BQ25186 Other Parts Discussed in Thread: BQ25180
I am having an issue with the BQ25186 that is giving me heartburn. I would like to use the ship mode to control power using a switch (NMOS) on TS/MR as is called out on the datasheet. It…
Part Number: BQ25186 Hi,
We are using the BQ25186 in a sealed, body-worn single-cell wearable. The cell-attached NTC into TS/MR is our only charge-temperature protection layer, so we need to know what the device does when that thermistor connection…
Part Number: BQ25186 Hello Team,
One of our customers is requesting pre sales support for part BQ25186DLHR. Please see following customer questions,
-------------
BQ25186DLHR: reset values, safety-timer fault and TS/MR filtering
Dear TI team…
Part Number: BQ25186 Hi Team,
We need support over a team's / Google meet call to configure the registers in BQ25186DLHR to detect the Battery Connect & Disconnect events. We are expecting a call because we have followed the steps shared by TI FAE but…
Part Number: BQ25186 Hi
Are there any similar ICs to the BQ25186DLHR but with higher current draw? Currently, the maximum current is 3A. Connecting peripherals at low voltage causes the device to reach the maximum current and shut down. Therefore, I…
Part Number: BQ25186
Hello, I'm writing since I believe that I have found an error in the datasheet (see image below).
In my driver, I've found that the POR value for this register to be 0x20 which matches the bits in the table, but above the table…
Part Number: BQ25186 Hello,
We are working through the code to handle the BQ25186 battery management IC. We were going to utilize a thermistor next to the coin cell to use the temperature shutdowns for charging and discharging.
Could you please confirm…
Part Number: BQ25186 Other Parts Discussed in Thread: BQ25620 , BQ25630 , BQ25630EVM , BQ25622EVM , PMP23456 , BQ25622 , BQ25622E I need a UPS function for a 5V 3amp device.
input - 5V 3A
Need battery charger with at least 1amp but 2amps preferred…
Part Number: BQ25186 Hi,
I cannot get information of how EXACTLY to communicate with BQ25186 with I2C. I assume it is the "classical" way: start,0xD4, offset, data, stop but is it autoincrementing offset ? can I do start,0xD4, 0x03, data1, data2, data3…
Part Number: BQ25186 Hello,
The datasheet for the BQ25186 says " 3.0V to 18V input voltage operating range for battery-to-battery charging, USB adapters, and high impedance sources "
The Recommended Operating Conditions state that Input Voltage Range…