Part Number: BQ25188 Tool/software: The BQ25188 datasheet in section 7.3.9.2 "Pushbutton Reset or Long Button Press Functions" refers to the /CE pin: "Toggling the /CE pin will restart the timer for the long press button when VIN is present." But the…
Part Number: BQ25188 Hi, Sir,
Please help to provide UL Certificate for BQ25188Y.
If there's no UL certificate, please provide other safety certificate to show that BQ25188 ould meet the standard IEC 62368-1 .
Thank you.
Customer : AMPACS COR…
Part Number: BQ25188 Other Parts Discussed in Thread: BQ25186 On page 31 of the data sheet the VBAT_CTRL registers appears to have an option to control the mythical PG_GPO pin. Is this a left over reference to another device, or have I missed something…
Part Number: BQ25188 I have some question about the BQ25188 TS function.
Does the BQ25188 NTC monitoring TS function have ICHG current limitation?
If the ICHG set to very low, like 20mA(or even lower 5mA?):
If VCOOL <VTS <VCOLD still reduce the…
Part Number: BQ25188 For the parameter Vsleep, we need to know the MAX value. Our buck converter feeding the linear charger has 2 possible values: 3.8V, and 3.4V. By knowing the max value of Vsleep, we will know when we need to switch Buck Vout from 3…
Part Number: BQ25188 Hello TI Support,
I am using the BQ25188YBGR in a battery-powered product and have encountered an issue with USB-C PD power sources. I would appreciate your assistance in understanding whether this is expected behaviour, a configuration…
Part Number: BQ25188 Hi,
my device can run from an adaptor or battery. I configure the BQ25188 to shut down by writing 0X51 to the SHIP_RST register.
I have a 10K resistor between TS/MR and GND and a push switch in parallel to wake the device up …
Part Number: BQ25188 Other Parts Discussed in Thread: BQ25186 Tool/software: Hello, I would like to use BQ25188 together with 1-cell LiFePo4 battery. But I do not understand the algorithm of the initial power-on. From the datasheet - after reset (switching…
Part Number: BQ25188 Tool/software: Hi
I want to check the leakage current between Vin(5V) and SYS , disable charge mode. could you help provide the current range ? and how to set IC ? thanks.
Part Number: BQ25188 Tool/software: Hello.
It isn't quite clear for me whether the BQ25188 can enter Shutdown mode by push button long press with VIN in its operation range. The only picture (Figure 8-12) of entering Shutdown mode by pressing the push…