Part Number: BQ25303J Hi,
Please help with the schematic review of all TI related components.
Battery charger 2.5A, and fuel gauge connected to external MCU.
If more information is needed, let me know.
Charger_V10.pdf
D1
ESD441DPLR…
Part Number: BQ25303J Tool/software: I am starting a design with the chip BQ25303JRTER.
In the datasheet it suggests to place a inductor (L1) reference Coilcraft XFL4020-102.
This inductor has polarity, but it is not stated anywhere in the datasheet…
Part Number: BQ25303J Tool/software: Hi,
I have a design using your IC BQ25303J, and as suggested from one of your employees from technical support ( BQ25303J: Typical Application circuit from datasheet ) I did not implement the schematic mentioned…
Part Number: BQ25303J Tool/software: Dear Team,
My customer is evaluating the BQ25303J in their application, and found that overdischarged batteries cannot be charged, and they are investigating.
Since the battery end voltage at the time of charging…
Part Number: BQ25303J Tool/software:
Dear Foram Members
I designed a charging circuit using BQ25303J. Please take a look at my circuit and share your feedback.
operating conditions:
Supply voltage: 5V via solar panel/ USB adapter
Battery voltage…
Part Number: BQ25303J Other Parts Discussed in Thread: BQ24105-Q1 Hi,
I'm using BQ25303J as battery charger in my design. But this part is not an automotive grade and operating Temp range in blw -40 to 85 degree Celsius.
Could you please suggest the…
Part Number: BQ25303J Tool/software: Dear Technical Service,
I followed the recommnedations from one of your colleagues about the BQ25303 and I designed this circuit:
Now what I got is that if I have D1 placed I see a significant voltage drop…
Part Number: BQ25303J Hi,
I am currently using the BQ25303J to charge a 5000mAh Lithium Ion Cell (21700). I have set the VBAT Reg at 4.2 V by connecting VSET Pin to ground using a 0 Ohm Jumper. The battery should charge should 4.2V, but
the charger…
Part Number: BQ25303J Tool/software: I'm stuck trying to calculate the thermistor resistors.
It seems to me that the equations for setting the resistors are wrong.
I get a negative number for R2
I gather there is no excel spreadsheet for this part…