Part Number: TPS25814 Other Parts Discussed in Thread: BQ25308 , TPS25730A Hi TPS25814 support team,
Upon reviewing the datasheet for the TPS25814, it appears to be designed solely for power sourcing. Can it be used in conjunction with the BQ25308 to…
Part Number: BQ25308 Tool/software: Greetings,
I have made the BQ25308 charger for my 1s Li ion cells at 2.6A charging current. It has worked when testing over a benchtop power supply. But when its connected to a generic AC/DC 12 volt 2A wall adapter…
Part Number: BQ25308
Tool/software:
Hi, TI expert
The customer is reviewing the BQ25308, and the battery used is 1 cell, lithium polymer.
The customer said that he conducted the test after forcibly discharging the battery completely, considering…
Part Number: BQ25308 DDevice_ESP Schematic-3.pdf When we work the device with only battery or only 5V IN, it works alright, However, when we connect the battery of 1800mAh and the 5V IN, the device heats up within 5-6 seconds to around 90 degree centigrade…
Part Number: BQ25308
Tool/software:
Hi, TI expert
The customer requested a schematic review using BQ25308.
[spec]
- Vin : 5Vdc
- Battery Voltage : 4.2Vdc / 1A or more
- Buck converter output : 4Vdc
Q1) Are there any issues? Is there…
Part Number: BQ25308 Hello,
There is a customer who is considering to use the IC. There is a folliwng question from her. Please help to answer to it.
Question; The datasheet says BLINKING frequency is 1Hz typ. with 50% duty cycle. Please let me know…
Part Number: BQ25308 Tool/software: Hi,
BQ25308 will charge the dead battery (cut off 2.34V)? iNHIBIT MODE will stop the charging .?
please confirm it .
Regards
Durga prasad
Part Number: BQ25308 Other Parts Discussed in Thread: BQ27427
We are workign on a 2000mAh battery with this device and are to use BQ25308 PMIC, with
fuel gauze BQ27427. Please review the schematcis. regards
Vivek
Part Number: BQ25308 Hello,
Could you please help to answer to the following customer's quetion?
Question : Please let us know the IC's self-consumption current in the following two cases.
Case1: When Enable is ON and the device is operating, but…