Part Number: BQ25504 Hi Team,
Were can I find the BQ25504_TRANS.LIB. I have checked the TI website but I could not find it.
Can you please provide the file?
Thank you.
Regards, May
Part Number: BQ25504 I'm trying to develop an energy harvesting app.
I intend to use VBAT_OK as a simple comparator output for VSTOR, and the threshold should be set below the VBAT_UV voltage. But the datasheet says, "VBAT_OK_PROG threshold must be…
Part Number: BQ25504 Other Parts Discussed in Thread: TINA-TI , TPS63900 Hi There,
I am building an energy harvesting system that uses BQ25504 as a first stage followed by TPS63900. I am unable simulate the systems since the BQ25504 only has model files…
Part Number: BQ25504 Hi, I found several problems when using BQ25504, forgive my English expression.
1. I don't need battery overdischarge detection, ie VBAT_UV is not programmed and that pin is left floating. During charging, once the battery voltage…
Hi Theagainmen,
The charger is discontinuous mode, PFM boost converter. So, like all boost converters and especially one in DCM, there is no easy formula to compute exact output power so we have use efficiency estimate and power balance. The max average…
Part Number: BQ25504 Hi teams:
Solar charging chip bq2504. The specification describes that the maximum boost swtich frequency is 1MHz.
When the chip works, the output voltage is adjusted through PFM mode.
Ask:
1. How does the chip control the boost operating…
Part Number: BQ25504 Hi
The customer design with BQ25504, the battery is a lithium titanate battery with a full charge voltage of 2.8V. But actually it stops charging at 2.34V.
Attached the schematic for your reference.
Please give some suggestions.
…
Part Number: BQ25504 The output i am getting from the power management device is not what is expected. I set up the simulation of the BQ25504 on TINA application from Texas instrument. The output is always less than input voltage. I set the input from…
Part Number: BQ25570 Other Parts Discussed in Thread: BQ25504 Hi,
I need to calculate the power consumption of ics in my design.
can you please help me to calculate the power consumed by these ic's when in operation - BQ25570 and BQ25504
Thanks in…
Part Number: BQ25504 Other Parts Discussed in Thread: CC1310 , Hi
My customer want to design with BQ25504, and they want to know BQ25504 collects solar energy, VSTOR is connected to CC1310, CC1310 working voltage is 3.3V.
Can CC1310 be directly connected…