Part Number: BQ25616 Other Parts Discussed in Thread: BQ25638 Tool/software: Hi
My customer are using Panasonic 18650 battery ,Vin(max) = 9V, Vin (Min) = 5V
When Vin = 9V, it need charge the battery with 4.2V/2A charging current. and also provide…
Part Number: BQ25616 Please can you assist with a review of our Power Path design.
1. If I don't want to use the D+/D- how must the circuit look?
2. Battery charging current +- 900mA
3. Power Limit +- 3000 mA (Maximum)
Part Number: BQ25616 Hello all,
I am using BQ25616 but I only need the battery charging functionality, not the boost regulator.
Do I need the inductor, Cout and a load? Can I leave the Boost related pins unconnected?
Thanks
Part Number: BQ25616 Other Parts Discussed in Thread: BQ24253 Hi support team, Three questions when changing from bq24253 to bq25616.
(1) Although bq24253 has been operated with EN1/2, does bq25616 automatically start charging after detecting power…
Part Number: BQ25616 Tool/software: Hello expert,
I saw this article on E2E.
The board we designed also does not use DP and DM pins, so both are connected to GND.
The current was smaller than the value set by the ILIM pin.
However, when both…
Part Number: BQ25616 Hi
I have a query need your help.
Does BQ25616 support Solar battery? The solar energy battery maximum 5.9V.
The BAT connect to 3.7V lithium battery.
Waiting for your reply.
Thanks
Star
Part Number: BQ25616 Other Parts Discussed in Thread: LM5013 , BQ25606 , BQ25185 , BQ25628 , BQ25620 , BQ25629 , BQ25638 , BQ25622 Hello Community,
I am working on the Quectel EC200 GSM module with one MCU on board for CAN communication.
The device…
Part Number: BQ25616 Other Parts Discussed in Thread: BQ25606 Are both BQ25606 and BQ25616 devices that can limit INPUT CURRENT LIMIT (IINLIM) to 500mA during USB SDP (USB500)?
Check the datasheet,
BQ25606 is
When “D+/D- Detection” is SDP, the…
Part Number: BQ25616 Other Parts Discussed in Thread: BQ25628 , BQ25620 , BQ25629 , BQ25622 Hi, I am developing a board that has the main power supply and the backup battery also, in case the main power supply gets deep discharged. Here the main power…