I think an easier first test case would be to remove the battery from the equation and figure out why I am unable to power the load through only VBUS.
But I just went ahead and ordered the BQ25616EVM as I think it would make troubleshooting easier on…
Hi Hayashi,
I just worked to double check with BQ25616EVM on bench and it appears the sequence discussed previously does not work to change Vset setting.
The device functions according to the datasheet. A input power cycle is needed for a change in Rset…
Hi Brian,
For this device the exact implementation of these pins cannot be shared publicly. Although I would recommend following the resistor power ratings used on the BQ25616 evaluation module (EVM) as reference on what the pins perform to.
Here is the…
Part Number: BQ25616 Hi Team,
I have received the bq25616EVM. But I can't find the corresponding bqz file. Could you please share me? Thanks.
Regards
Olin Zhang
Part Number: BQ25616 According the the BQ25616 datasheet Quiescent battery current could be as low as 9.5uA.
I have followed the datasheet and the datasheet of the BQ25616EVM EVALUATION BOARDS and made a prototype.
the current reading on the battery line…
Part Number: BQ25616 Other Parts Discussed in Thread: , BQ25606 Hello, Trying to implement a BQ25616 solution for a standalone LiHV single cell (4.35V) battery charger. No system powering, just battery charging. As opposite to BQ25616EVM, no separate leds…
Part Number: BQ25616 Hi all
My customer is evaluating the BQ25616 using the BQ25616EVM and they have this setup:
- No supply on VBUS
- Battery not charged
- Battery almost empty (< 3.0V, emulated with a power supply)
- USB OTC Boost function activ…
Part Number: BQ25616
I would appreciate your review of the attached schematic and comments/answers to the following details that arose during the design process.
Given circuit will be used with generic 5 VDC supply input rather than USB power is it…