Part Number: BQ25616JEVM Hi team,
Customer request to modify the charging profile as below,
T1 at 0 degree C, and T5 at 55 degree C.
We would like to know
What will T2 and T3 become?
How to set T1 and T5 as request?
Part Number: BQ25616JEVM e2e.ti.com/.../bq25616jevm-bq25616j
The status of the original thread was mistakenly set to Resolved, but it has not been resolved yet
A new datasheet has been issued. It was January 2021 when I contacted TI-JAPAN and decided…
Part Number: BQ25616JEVM In the past, I had a problem with the bq25616j charging circuit and made an inquiry. It seems that the page cannot be written anymore, so I will contact you again.
After that, as a result of testing with various settings, when…
Part Number: BQ25616JEVM This is a continuation of the question about the full charge detection of the BQ25616J that I inquired about last time.
Instead of asking the question on BQ25616JEVM, when BQ25616J is mounted on this board, built into the product…
Part Number: BQ25616JEVM I have an inquiry about the operation of BQ25616J.
A strange phenomenon occurred while the product was placed in a small constant temperature bath and evaluated.
Charging in a 25 ° C setting environment: OK (A full charge signal…
Part Number: BQ25616JEVM Dear team
The attachment is the BQ25616J hardware setting,
R12, R20, R24, R22 have to modify the resistance and adjust the value of the variable resistance group, JP11, JP12 are shorted, JP21 is grounded.
How to calculate the T1…
Part Number: BQ25616JEVM Dear team
When The customer tested the BQ25616J EVM board in an environment of 25 degrees Celsius, They found that the current will oscillate when the battery voltage is between 4.34V and 4.35V . They would like to know what is causing…
Part Number: BQ25616JEVM Dear Support team!
The charger IC BQ25616J monitors the discharge current through the BATFET Q4. When there is an overload or short the BATFET will turn off.
My questions are:
1. What is the minimum and typical time the defined…
Part Number: BQ25616 Hi
I have the same query like the following post.
https://e2e.ti.com/support/power-management-group/power-management/f/power-management-forum/992831/bq25616-stat-pin-blinking-frequency/3669176?tisearch=e2e-sitesearch&keymatch=C_V…