Part Number: BQ25618 We have been directed by TI customer support to request a private time-sensitive dicussion with an FAE on an issue with BQ25618. Please let us know how to privately contact an FAE on this topic.
Thank you
John
Part Number: BQ25618 Hi TI,
We're using the BQ25618 in our device, and want to be able to put the device into Ship mode + turn off Vsys with VUSB connected. We want to confirm the that the following ordering of events is valid, and does not put the…
Part Number: BQ25618 Hello,
Our custimer is facing on an issue of BATFET to VSYS overcurrent without input source. Though he does not face on BATFET off by IBAT > ISYS_OCP_Q4 yet, he is concerned about BATFET fully off then his system freezing. When…
Part Number: BQ25618 Other Parts Discussed in Thread: BQ25638 , BQ25798 Hi,
I will start a design using the part number BQ25618YFFR, and I would like the design to have the option to connect either a USB adapter or a solar panel to the VBUS input. Is…
Part Number: BQ25618 Hello,
I would like to make sure EN_HIZ reset (trun to default state) condition. Is my understanding below correct for EN_HIZ=1 (HIZ mode) to 0 (HIZ disable) condition ?
REG_RST=1 or Watchdog timer expired.
VBUS "rises" above…
Part Number: BQ25618 Tool/software: Hi Team
My customer side want to set T5 as 50 degree but datasheet condition is T5 = 60.
do it have any requirement to change to ratio of T2/T3? because the resistor divider ratio is different. is T2/T3…
Part Number: BQ25618 Hi Team,
I would like to confirm with you if we use this sequence to enter shipping mode, is there any hardware risk?
Plug in Adapter
Ensure Charger IC detects VBUS
Set BATFET_DIS =1
BATFET_RST_WBUS =1
5 Remove Adapter…
Part Number: BQ25618 Other Parts Discussed in Thread: BQ25638 Tool/software: Hi Team
do we have any lower Iq solution for replace BQ25618?
it's 9.5uA but customer hope it can lower as 5uA.
BRs
Brian
Part Number: BQ25618 Hello,
Our customer has a question if BQ25618 build in BATFET soft on function during the system power up from battery only.
The back ground of this question is the customer wants to know if BQ25618 can prevent from rush current…
Part Number: BQ25618 Hello,
Our customer has a question of Narrow VDC (NVDC) voltage max as his design reference. Even though we asked similar question before and we cannot specify the max in the datasheet, would it be possible to let us know the expecting…