Part Number: BQ25619E Reading BQ25619E datsheet I didn't understand which is the behaviour of system voltage when nop ower is present on Vbus pin but there is a battery charged connected at VBAT pin. In this situation the Power Path Management connects…
Part Number: BQ25619 Hi Team,
My customer have a voltage accuracy question for BQ25619 and BQ25619E.
When the register 0x04[7:3] is set to "00110" (4.1V), we measure differential Vreg on same FW, HW and temp.
The battery charge to 4.086V on BQ25619E…
Part Number: BQ25619E The BQ25619E has a limited system supply capability. We need to draw about 6A from the battery for short periods (about 200mS). Is it acceptable to bypass the chip load circuitry by connecting a schottky diode from the battery positive…
Part Number: BQ25619E Other Parts Discussed in Thread: BQ25619 , Hello,
I see that the BQ25619E is a boost-less version of the BQ25619. What hardware and firmware/register changes should we be aware of when moving from the BQ25619 to the BQ25619E? …
Part Number: BQ25619E Hi,
Good Day. I have a customer who is working with BQ25619E. Please see below his query for your reference. Thank you very much.
In the BQ25619E datasheet it is mentioned Isw = 1.8A , Why it is limited to this much current as…
Part Number: BQ25619E Other Parts Discussed in Thread: BQ24259 ,
Hello, I have problem with bq25619E I used is as more available replacement of bq24259 which works great with same board and topology. When VBUS is connected or disconnected I have MCU…
Part Number: BQ25619E Other Parts Discussed in Thread: BQ25619 , BQ24072 , BQ24232 , BQ24250 Hi team,
Customer is looking for 1 cell charger IC which with interface I2C, WQFN package, NTC monitor, power path switch node to system load for 1cell +3…
Part Number: TPS55288 Other Parts Discussed in Thread: BQ25619E , Dear TI people,
I would like to know which kind of process I must follow to use some of your parts (for example DC/DC converter TPS55288 and battery charger BQ25619E) in implanted medical…
Part Number: TPS2116 Other Parts Discussed in Thread: TPSM53602 , BQ25619E Hi!
We have an application which has two inputs, both at 5V. We are using the TPS2116 in priority mode with MODE tied to VIN1.
VIN1 is generated by a TPSM53602 from 9V DC,…