Part Number: BQ25628E Hello, can we please obtain a copy of the IEC 62368-1 CB Certification for the BQ25628E to add to our pack for certification.
Thank you,
Dan.
Part Number: BQ25628E Tool/software: Hi, this question follows from one asked in this post , about detecting the presence of a battery with this device. I am trying to do the same in my design, and have followed the procedure outlined in Part 1 of the…
Part Number: BQ25628E Tool/software: Dear TI,
We are using the BQ25628E in our design but have been unable to find a Linux driver sample for this PMIC. The existing driver at this link: www.ti.com/.../BQ256XXSW-LINUX does not seem to support the BQ25628E…
Part Number: BQ25628E Hi I have encountered the following issue: When setting my PS to 6V I am able to sustain a charging current of 1A. When setting my PS to 5V the VINDPM bit is rising and I reach ~150mA charging current. When using a USBC at 5V the…
Part Number: BQ25628E Hello! I am currently working on a product using the BQ25628E to charge a RRC1130 4.35V LiPO battery. VBUS is being provided by USBC-PD and the BQ25628E is being controlled by a MAX77958 PD controller IC. PDO's for 5V, 9V, 12V and…
Part Number: BQ25628E Tool/software: I am using the BQ25628E and I encountered the following issue: When I disconnect VBUS from the system while the battery is still connected to BAT the reported IBAT from REG0x2A_IBAT_ADC drops to 0 despite my system…
Part Number: BQ25628E Tool/software: Based on the application note, our BQ25628E schematic is as below. Please advise if there is any issue.
-CHARGE/CHG_status/CHG_INTn/SDA/SCL/CHG_CEn/CHG_ISET are connected to the host.
-TS is connected to the…
Part Number: BQ25628E Tool/software: Hi,there, here is my schematic, using 25628E, pls notice that , R7 has been changed to 2K from PCBA。 AND
R8/R9 has been change to 5.23K and 30.1K, a NTC@10k is used。 the problem is now that the charging current is…
Part Number: BQ25628E Other Parts Discussed in Thread: , BQ25628
Hi! On our board, we're using a BQ25628E to manage charging a li-ion battery while handling system voltage.
During our testing, we've observed the IINDPM_STAT bit being raised, and as…