Part Number: BQ25630 We see BQ265XXSW-LINUX but didn't see BQ25630 listed in its ID array. Can BQ25630 use the driver? Or any other reference driver provided? Thanks.
Part Number: BQ25630 Hi Sir,
My customer is designing BQ25630 in their Headset product. Is there any driver support on BQ25630? We see BQ265XXSW-LINUX but didn't see BQ25630 listed in its ID array. Can BQ25630 use the driver? Or any other reference…
Part Number: BQ25630 Hi Team
There is oscillation in charging efficiency of BQ25630 during the CV phase, Do you have any ideas about what could be causing this? Thanks.
The charging efficiency oscillation observed with the BQ25630 during the CV phase…
Part Number: BQ25630 Hi Team,
Could provide the maximum duty cycle for the buck adjustment on the charging IC BQ25630?
We would like to calc min working voltage. Thanks.
Part Number: BQ25630 Other Parts Discussed in Thread: BQ25895 , Hello, on my current version of battery powered product I was using the BQ25895 battery charging IC. It had one handy pin - the DSEL - that was controlling the USB multiplexer to hand over…
Part Number: BQ25640 Other Parts Discussed in Thread: BQ25630 , Hi
Is there any advantage to using the BQ25640 over the BQ25630? The new version of the BQ25630 datasheet includes a layout recommendation that we did not follow on our board (the new datasheet…
Part Number: BQ25630 I have an application where I need a single cell lithium charger that will be only a sink but will need to communicate to an intelegent host or a USB-C wall charger that it needs to increase voltage on the VBUS line to 9V from the…
Part Number: BQ25630 Other Parts Discussed in Thread: BQ25638 Tool/software: Hi Team,
I need suggestions for the following questions.
Please help.
Thanks.
1. For power saving design, the host will shut down after finishing I2C data setting and…
Part Number: BQ25630 Tool/software: Hi Team,
I know the 15W normally means 5V/3A output capability.
Why it supports up to 18V input voltage even only 5V appears in normal operation?
Does TI think USB power input needs 18V rated voltage for safe…
Part Number: BQ25630 Hi BQ25630 support team,
As described in "9.2 Typical Application" of the datasheet, we are considering connecting an LED between the /PG pin and the SYS pin.
The conditions for the /PG pin being HIGH or LOW are listed in "8.3…