Part Number: BQ25703A Other Parts Discussed in Thread: BQ25723 Hi
Can you help to determine whether the BQ25703A can meet the following requirements?
Case1: The POGO PIN end is connected to an external power bank, BUS_P input, and VSYS supplies power…
Part Number: BQ25703A
A customer has a question that when using a 20V/2.25A (45W) type-C adapter to charge a 4100mAh battery (3S) with 0.7C (ChargeCurrent: 03/02h = 0x0C00) under the condition of S5 (system power consumption<1W), but the charging…
Part Number: BQ25703A Other Parts Discussed in Thread: BQ25703 , , BQSTUDIO HI
A customer has a question about setting the battery to enter shipping mode. Generally, the battery only needs to be supplied with a certain voltage (the current can be very small…
Part Number: BQ25703A Other Parts Discussed in Thread: BQ25700 Hi TI Teams,
We have some question about the register setting of BQ25703A, that is, we want to set the SRN for Shipping mode(EN_SHIP_DCHG), from the datasheet we can learned that this function…
Hi Lumina,
Since there are no replies from you in a while, I am assuming the issue is resolved and I will close the thread. If you need further assistance, feel free to get back to us on the TI E2E forum.
Best Regards,
Jacob
Part Number: BQ25703A Other Parts Discussed in Thread: BQ25703 , hi:
Bq25703 A+2 lithium batteries+CW2017 battery level detection,
The battery voltage read now is abnormal.
The customer has configured their own parameters and found that the chip will keep…
Part Number: BQ25703A Hi TI Teams,
One of our customer's application needs to control the battery level between 80% and 90%, and stop charging when the battery level is higher than 90%. At this time, the load can only be powered by the battery (adapter…