Part Number: BQ25708 Hi,
I have a design based on the BQ25708 chip which is meant to be able to charge 2s and 4s batteries. Additional circuitry has been implemented to determine whether 2s or 4s charging is required, and a microcontroller applies the…
Part Number: BQ25708
We have a product that has incorrectly connected a voltage divider circuit (2 resistors) from a 12 volt battery to the CELL_BATPRESZ pin. If the battery is depleted at power up, the CELL_BATPRESZ pin is too low and the SYSOVP threshold…
Part Number: BQ25708 Other Parts Discussed in Thread: BQ25700A Battery charger team,
Which EVM do you recommend as a starting point for work with BQ25708?
Thanks, Darren
Part Number: BQ25708 Hi all,
Does BQ25708 support as Level II battery charger as per the Smart battery charger specification 1.1?
I am trying to find out a Level II battery charger from TI road map with the below requirements.
Level II Battery Charger…
Part Number: BQ25708 Question: what is the state of BATDRV, and therefore BATFET, when the battery is removed?
Background: we have an instance in which there is a front panel switch to isolate the battery from the circuit, as illustrated below.
If the…
Part Number: BQ25708 Other Parts Discussed in Thread: BQ25700 Hi
Based on the imx6 platform using bq25708, there are now null pointer bugs as follows:
[ 2.300418] [bq25700] bq25700_init_device: Charger Enabled Successfully! [ 2.311822] [bq25700] bq25700_init_device…
Hi Christian,
I was also checking the information on the E2E site, but your answer helped us to clear up some of the questions I had in previous threads.
(+) BQ25708: SMBUS 1.1 PEC compliant? - Power management forum - Power management - TI E2E support…
Part Number: BQ24721C Other Parts Discussed in Thread: BQ25708 Tool/software: Hello,
according the datasheet of BQ24721C the minimum battery charging voltage is 9V (register 0x15), this is for the most 2 cell Li ion battery packs to much. As possible…
Hi, Volk,
We have developed a schematic checklist to assist you on the schematic review. Please check it out.
e2e.ti.com/.../faq-bq25730-faq-how-do-i-ensure-the-charger-schematic-is-satisfactory-is-there-a-schematic-checklist-for-ti-buck-boost-controllers…
Hi all, The buck-boost charger controller BQ25710, BQ25720 and BQ25730 is a host-controlled device. It doesn’t have a termination current setting and cannot terminate the charging by itself. After the charger enters CV (constant voltage) mode and charge…