Part Number: BQ25710 Hi AE.
We would like to understand why the system voltage suddenly drops to 6V
under the following conditions:
1. The EC writes 0x14 to set the charging current to 256 mA.
2. CELL BATPRESZ keep 4 cell status
3. The system…
Part Number: BQ25710 Hi AE,
Please help provide efficiency report for the following conditions.
1.Vin : 20V , Vout :18V ,Iout : 1mA~10mA
2.Vin : 20V , Vout :13.5V ,Iout : 1mA~10mA
Best Regards
Part Number: BQ25710 Other Parts Discussed in Thread: BQ25700 Dear TI.
Hi. I'm Dongwon Lee of Samsung Electronics.
We are trying to charge with Bq25710 chipset, but it doesn't work yet.
We are setting as register like below:
line 930: \par bq25700_init_charger…
Part Number: BQ25710 Hello E2E Experts,
We are proceeding with the model using the BQ25710 IC. For charge/discharge verification, we need a "buck off" function where the current from the travel adapter is not supplied while the travel adapter is connected…
Part Number: BQ25710
Hi Ti
I want to know, the BQ25710 recharge level 95% is battery voltage drops or RSOC from 100 to 95 ?
That is normal. The charger stops charging automatically when the battery voltage reaches the charge voltage() target. It…
Part Number: BQ25710
Hi team,
Let me ask about 0x12[1] EN_IDPM. I used the BQ25710EVM to check this feature. If I set 0x3F to 2A and 0x12[1]=0b (other values are POR), the IBUS can be more than 3A constantly.
Are ILIM2 and Icrit disabled if EN_IDPM…
Part Number: BQ25710 Other Parts Discussed in Thread: PMP22419 , CSD87355Q5D Using the reference materials for the PMP22419 board from the official website, I hand-soldered a motherboard myself and used the BQ25710, following the reference materials exactly…
Part Number: BQ25710
Hi Ti
4S cell battery with the Upper limited charging voltage 18.12V is used in my board, should I write 0x15 = 0x46C8 (18120mV) or 0x41A0 (16800mV) ?
Part Number: BQ25710 Other Parts Discussed in Thread: TIGER Tool/software: Hi Team,
From datasheet, I can find below description for learn mode. Beside that, is there any more detailed introduction material for learn mode?
When the device is in learn…
Part Number: BQ25710 Other Parts Discussed in Thread: TIGER , BQ25770 Tool/software: Hi team,
I want to know when BQ25710 move from Buck to Buck-boost and Buck-boost to Boost vice versa. Competitor's charger depict visible image like Vin=90%*Vsys is…