Part Number: TPS25751 Other Parts Discussed in Thread: BQ25713 , , BQ25713B Hello,
We are using the TPS25751 and BQ25713 B in a design. The USBCPD Application Customization Tool only has BQ25713 as an option which has a different I2C address than the…
Part Number: BQ25713B Other Parts Discussed in Thread: BQ25703A , BQ25713 , TIGER Hi
Does the BQ25713BRSNR chip have a trim charge function? Or suggest other product?
Battery: 4S2P (14.8V nominal / 16.8V full / 52.2Wh)
For example, with a BQ25703A…
Part Number: BQ25713B Other Parts Discussed in Thread: BQ25713 , In looking at the comparison chart I see that the only difference between the BQ25713 and the BQ25713B is in the "Device Address" field.
BQ25713 = 6Bh
BQ25713B = 6Ah
What is the difference…
Part Number: BQ25713B Other Parts Discussed in Thread: TPS25750 , , BQ25713 Dear Suppot Team,
we are currently debugging a board with the combination of TPS25750 and the BQ25713B. In my understanding the TPS25750 supporting only the BQ25713 (without…
Part Number: BQ25713B Other Parts Discussed in Thread: TIGER Tool/software: Hi Experts,
My name is Antonio and I'm struggling with the charging IC BQ25713B. I'm trying to charge the 1S cell 21700, my power supply is 12V DC.
I programmed it with the…
Part Number: BQ25713B Other Parts Discussed in Thread: BQ25713 , TIGER Tool/software: Hi,
I have a question about if is it possible to connect two or more BQ25713 in parallel to charge a LiFePO4 battery with a high current.
Kind regards,
Antonio…
Part Number: BQ25713B Other Parts Discussed in Thread: TIGER Hi TI team:
BQ25713B can be set to Direct Through Mode (PTM). What is the maximum output voltage that VSYS can reach in PTM operating mode?
If the output voltage of VSYS remains at 23V,…
Part Number: BQ25713B Other Parts Discussed in Thread: BQ25713 , TIGER Tool/software: Hi,
My name is Antonio López and I have a few questions about the BQ25713B:
Which is the difference between BQ25713 and BQ25713B?
Can I make my own PCB with…
Part Number: BQ25713B Other Parts Discussed in Thread: BQ25713 Hi
I have a query need your help.
When I remove the adapter, r egisters cannot be read and written when in boost mode. Does it normal?
The register setting as below:
struct bq257xx_reg_st…