Part Number: BQ25720 Hi Team,
Can i use BQ25720 as a standalone charger IC without Host?.If it is possible Then what is the limitation in performance without Host controller.
Part Number: BQ25720 Other Parts Discussed in Thread: BQ2570 , Hi Team,
My system load for 12V Isys =7A + I chrg = 4A = Total 12V @ 11A approx. So i am going to use 150W charger . Do BQ2570 support input current 19V @ 7.8A .
Part Number: BQ25720 Other Parts Discussed in Thread: BQ25710 , Hi Expert,
I found the BQ25710 PTM mode need some process to enable. But BQ25720 did not mention it, does BQ25720 activation require the same process?
Far
Part Number: BQ25720 Other Parts Discussed in Thread: BQ25730 , BQ40Z50-R2 Dear TI Teams,
We have two projects that require fast charging, and we need to determine the selection of charging ICs, both of them are the details are as below:
Project 1:
1…
Part Number: BQ25720 Other Parts Discussed in Thread: BQ25710 , Hi Tiger,
I found the E2E thread as below, you mention the power up process may take 200ms, a ny write during this time may be lost. The delay 200ms is base on CHEG_OK assert or VBUS?
https…
Part Number: BQ25720 Other Parts Discussed in Thread: BQ25710 , Hi Team,
What is the input current limit for BQ25710 and BQ25720.Which means what is the maximum current supported from 19V AC/DC adapter. From BQ25720 reference notebook design i come to know…
Part Number: BQ25720
Hi Expert,
Want to know if enable the Low Power Mode when adapter is presented, what impact will it have? Will cause BATDRV be asserted?
Far
Part Number: BQ25720EVM Hi Team,
What is the use of CHG_OK signal here. I simulated the same in PSPICE and unable to control the input voltage with CHG_OK pin.Help me out to understand the logic.