Part Number: BQ25730 Other Parts Discussed in Thread: , DAC53701 Tool/software: Dear TI team.
I have a basic and general question about your battery charger solutions, specially the BQ25730.
We are currently working on a design which should work as…
Other Parts Discussed in Thread: BQ25730 , TPS25751 Tool/software: Hello experts,
I was not so sure which device to post so I just selected BQ25730,
But do we have a E-marker IC for 60W charging solution, not for USB-PD but for SMPS, in any of our…
Part Number: BQ25730 Tool/software: Hello experts,
I had a quick question, is there a IC or charging method that is faster than CC/CV charging for 60W?
My customer was looking for 60W (17.54V 3.4A) solution so I suggested BQ25730, but they asked if…
Part Number: BQ25730 Tool/software: Hi team,
I would like to check with you about BQ25730 broadcast behavior:
1. Will BQ25730 report the device MCU status over I2C in both charging and sleep states?
2. Will BQ25730 report fault status(if met)…
Part Number: BQ25730 Tool/software: When charging, is the Voltage to the system adjustable? For instance if the voltage in is 12V can the Voltage to power the system be set to 3.7V?
Part Number: BQ25730 Tool/software: I am feeding 14V to the charger via VBUS. VSYS_MIN is set to 9.5V. The battery charges at 500mA as expected up to 9.5V. However, at this point it stops charging. My expectation is that it should charge to full pack…
Part Number: BQ25730 Tool/software: Hello experts,
Currently my customer is reviewing BQ25730 for their robot vacuum project.
Right now they are trying to control BATFET on/off based on register map explanation on datasheet.
However, when they tried…
Part Number: BQ25730 Tool/software: Hi Team,
May I have your support to review below sch? Thanks!
1. this project uses a 4S2P configuration. Please help review the schematic
(Load power supply process: During charging, the input directly powers…
Part Number: BQ25730 Tool/software: Dear Team,
We are using BQ25730 for a Medical device.
19V is my VBUS and 4S Li-Ion Battery pack has been configured for the device
Unfortunately BQ25730 is not waking up from both VBUS and VBAT.
I have personally…
Part Number: BQ25730 Other Parts Discussed in Thread: TPS25751 Tool/software: We are currently implementing a USB-PD based battery charging and system power solution using BQ25730 in conjunction with TPS25751 for a project requiring:
System Load: 5A…