Part Number: BQ25750 Tool/software: Hi Team,
My customer is using BQ25750 and they wish to control BATFET connection manually. May I know how to meet this requirement? I don't find related control in register map, Thanks.
Best Regards.
Wiky
Hello Ben,
I'm not sure where that ripple would be from without more information.
By the way, how are you measuring the HSgate signal?
Best Regards, Ethan Galloway
Part Number: BQ25750 Other Parts Discussed in Thread: BQ25820 Tool/software: Hello,
the reference manual "SLUSDY3 – DECEMBER 2023" refers to EN_VREG_TEMP_COMP twice, inside Table 8-25 and Table 8-39.
But they both are just a reference, can…
Hello Ben,
Thanks for being patient with this.
From our testing, a lower resistance is better and a capacitance of 8nF to 20nF works well for the circuit.
Also, it looks like the power path function of your circuit is working well. Let me know if you…
Hi Ethan,
I just figured out that the battery I am using is special one (BB-2590/U). It is combined of two independent battery packages, which I connected in series before charging with the BQ25750.
I think now that if the two are not fully charged and…
Part Number: BQ25750 Other Parts Discussed in Thread: BQSTUDIO
Tool/software:
Hello,
I'm using the BQ25750 for a new design which have an integrated 50V 15A battery charger, but I have some difficulties to make it work correctly.
Do debug it, I made…
Part Number: BQ25750 Tool/software: Hello,
Our customer has a question if BQ25750 can support Dynamic Power Path Management function that is supply the system load current by both Input power source and the battery. would you please help our customer…
Part Number: BQ25750
Tool/software:
By default, the BQ25750 has an automatic power path switchover. When the VAC power is out the of range set by the ACUV/ACOV resistors, system power will change to VBAT. When VAC is in range again, system power will…
Part Number: BQ25750 Other Parts Discussed in Thread: BQ76942 , BQ25756 Tool/software:
Hi Team,
Attached is an image showing the block diagrams of two ICs used in our system. Our project is a power bank with a 240 Whr capacity, configured with a 5S…
Part Number: BQ25750 Other Parts Discussed in Thread: BQ25780 , INA214 , , INA114 Tool/software: Hi,
I´m designing an PCB with the BQ25780 and have some strange behaviour with the current measurement.
In my first design I realized, that the measurement…