Part Number: BQ25758A Other Parts Discussed in Thread: BQ25750
I am designing a bidirectional 24V system with a 16x 600F Supercap module (0V to 40V).
We need to:
Charge: CC mode from 24V rail at 10A–20A (starting from 0V).
Discharge: Deliver…
Part Number: BQ25758A Hi Teams,
While testing OCP function, we found that the BQ25758A does not completely shut off the output. Could you please help confirm what might be causing this behavior?
Our circuit is configured with RIOUT = 4.99 k. The measured…
Part Number: BQ25758A Hi Experts,
I am checking the customer design below and I need help troubleshooting.
The issue was the design worked correctly in Boost mode, boosting 5V VIN to 10V Vout with expected switching frequency and duty cycle. But the…
Part Number: BQ25758A Other Parts Discussed in Thread: BQ25758 Hi Teams,
We are using BQ25758A with buck-only mode, please help to check following questions, thanks.
How to connect pin HIDRV2 and LODRV2? floating?
We are using 4.7uH inductor,…
Part Number: BQ25758A Other Parts Discussed in Thread: BQ25758 Hi Team,
Could you please help confirm the following questions? Thanks.
We plan to use bypass mode in a PD 20V/5A application.
Is bypass mode enabled simply by setting Register 0x1E…
Part Number: TPS26750EVM Other Parts Discussed in Thread: BQ25756 , BQ25758A , BQ25756E , , TPS26750 , TPS26750A Hi,
Is there a way to configure the TPS26750EVM to be used with the BQ25758A EVM instead of BQ25756 or BQ25756E EVMs?
The USBCPD Application…
Part Number: TPS65994AD Other Parts Discussed in Thread: TPS65994BG , BQ25758A
There is a Gaming Dock design with TPS65994BG and BQ25758A, below is the schematic of this dock PD solution, full_FW_v8.zip this is the FW and project that provided by FAE…
Part Number: BQ25758 Other Parts Discussed in Thread: , BQ25756 Hello, the description of TS/NC pin in datasheet states: "To enable pin functionality, set EN_TS register bit to 1". But in register description there is no EN_TS pin.
My question is will…