Part Number: BQ25790EVM Tool/software: Can you share the altium design for the evaluation module to understand better the stackup constrain and layout rules?
Regards
Part Number: BQ25790EVM Other Parts Discussed in Thread: EV2400 , BQSTUDIO Hi team,
Our customer uses MCU to write SDRV_CTRL=10 in BQ25790EVM to enter ship mode but failed. There is no adapter, REG_RST=1 or OTG enable at this time.
I duplicated this issue…
Part Number: BQ25790EVM Hi TI Support,
I'm developing a battery charger using the BQ25790EVM board, and believe to have found a few errors in the datasheet:
1) Setting VINDPM should be 4.000, not .4000. Other section using other I2C tool shows 4.…
Part Number: BQ25790EVM Would like to know if Layout design file is available for BQ25790EVM.
So that we directly us the layout and quickly develop our prototype. We have BQ25790EVM and it works well in our application.
Regards,
Part Number: BQ25790EVM Hi,
I have problems with Shipping mode operation using BQ25790EVM (BMS027) Evaluation Module with BatteryManagementStudio-1.3.111_Build1 and EV2300/2400 Interface Board, selected Chapter_2_01-bq25790_92.bqz target.
Please see attached…
Part Number: BQ25790EVM Other Parts Discussed in Thread: BQ25790 , EV2400 I started work with the BQ25790 charger, connected BQ25790EVB setup. It works good and charges the battery. when I connect my PC to the EVB using the EV2400 module by I2C the GUI responses…
Part Number: BQ25790EVM Other Parts Discussed in Thread: TPS25750 , BQ25790 , , TPS25750EVM , TUSB320EVM Hi Team,
Is it possible to hook up USB-C on Connector V1 (J1). On more in detail, Is it possible to connect plus and minus to J1 and D+ and D- on for…
Part Number: BQ25790EVM Hi,
Exploring BQ25790EVK connected via USB_TO_ANY and associated Cloud GUI.
ADC IBAT current reading shows charge current, but I can't see discharge current readings, it shows 0.0 A.
Is there any chance to get hold of this…
Part Number: BQ25790EVM Other Parts Discussed in Thread: BQ25790 Hello TI
Short question
REGN ( internal LDO ). Pge 14/133 in DS: Iregn 30mA@5Vbus.
In application design from DS the internal LDO is driving a LED ( R =2.2K ) in series.
General quesiton…
Part Number: BQ25790EVM Other Parts Discussed in Thread: BQSTUDIO , USB2ANY , EV2400 , BQ25790 , BQ24179
According to a similar post:
BQSTUDIO only works with EV2300/2400.
GUI Composer, which we will be using with all new devices, only works with USB2ANY…