Part Number: BQ25798 Tool/software: Hi teams,
Due to the fact that some older chargers can only support 5V/0.5A current, if it is inserted into a speaker, the charger will output the maximum current to the speaker, causing overload. We set the "REG05_input…
Part Number: BQ25798 Other Parts Discussed in Thread: BQ40Z50 , , BQ40Z50-R2 Tool/software: Hi there—our product comprises a 1S battery pack implemented using a BQ40Z50, and charged by the BQ25798. The pack implements its own precharge path—the schematic…
Part Number: BQ25798 Tool/software: Hello everyone,
I'm currently working on an Electrical power System project. I've successfully used a single BQ25798 charging IC, and it operates as expected. Howerver, when I try to use 2 ou 3 bq25798 in parallel…
Part Number: BQ25798 Tool/software: Hello!
My team and I are currently working on integrating the BQ2598 Charger Chip into our hardware design. We are using the BQ25798EVM board for reference to verify our readings and to identify any discrepancies…
Part Number: BQ25798 Tool/software: Backup mode is expected to work as follows:
Host software sets (arms) EN_BACKUP=1 while input source is attached at VBUS
Input voltage fails below backup mode trigger point = %*VINDPM
Backup mode engages setting…
Part Number: BQ25798 Other Parts Discussed in Thread: TPS25221 , Tool/software: hello,
The customer needs to charge the supercapacitor with an input voltage of 20-30V, and requires the chip input voltage to be above 40V, the charging voltage is 0-20V…
Part Number: BQ25798 Other Parts Discussed in Thread: BQSTUDIO , USB2ANY , EV2400 , TPS25751 Tool/software: Hello,
I have connected following supply for BQ25798 then how its work and what's my output.
1. If I give 5V USB type-C and 12V Solar As input…
Part Number: BQ25798EVM Other Parts Discussed in Thread: BQ25798 Hi Team, In our design, VSYS is used to power an external PMIC (PCA9450C), which typically expects a stable 5 V input.
Our battery configuration has 2-cell which give total 8V output …
Part Number: BQ25798 Other Parts Discussed in Thread: TPS2120 Hi
My customer got some questions can you help
There are safety timers for trickle charge, pre-charge, and fast charge modes. What will happen if the safety timer expires? Will the charger…